DDR3 memory calibration in a imx6d board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DDR3 memory calibration in a imx6d board

3,040 次查看
aicastell
Contributor II

Hi,

I'm trying to configure DDR3 RAM memory to start the calibration test in a i.MX6D board.

The problem is I don't see the output generated by the stress test in the debug console UART1. This is the first time I try to do this task, so probably I havent configured some register properly.

The memory connected in my custom board is a 1GB Micron with Part Number: MT41J256M16HA-125:E. According to datasheet, the micron memory has this configuration:

    Configuration:  32 Meg x 16 x 8 banks

    Refresh count:  8K

    Row addressing: 32K

    Bank addressing: 8

    Column addressing: 1K

    Page size: 2KB

    CK: 1.25ns

    CL: 11

    Target RCD-RP-CL: 11-11-11

    RCD (ns): 13.75

    RP (ns): 13.75

    CL (ns): 13.75

    Data Rate (MT/s): 1600

    RAS (MIN) Idd: 28

    RC (MIN) Idd: 39

Hardware is designed with just one single Chip Select.

In order to setup control registers I am using I.MX6DQSDL DDR3 Script Aid V0.10.xlsx aid script with this values:

    Device Information

    ===================================================

    Manufacturer:                   Micron

    Memory part number:             MT41J256M16HA-125:E

    Memory type:                    DDR3-800

    DRAM density (Gb):              2

    DRAM Bus Width:                 16

    Number of Banks:                8

    Number of ROW Addresses:        15

    Number of COLUMN Addresses:     10

    Page Size (K):                  2

    Self-Refresh Temperature (SRT): Normal

    CAS READ latency (CL)           11

    tRCD=tRP=CL (ns)                13,75

    tRC Min (ns)                    39

    tRAS Min (ns)                   28

    System Information

    =================================================

    i.Mx Part:                      i.Mx6D

    Bus Width:                      32

    Density per chip select (Gb):   8

    Number of Chip Selects used:    1

    Total DRAM Density (Gb):        8

    DRAM Clock Freq (Mhz):          400

    DRAM Clock Cycle Time (ns):     2,5

    Address Mirror (for CS1):       Disable

    SI Configuration

    =================================================

    DRAM DSE Setting - DQ/DQM (ohm):        48

    DRAM DSE Setting - ADDR/CMD/CTL (ohm):  48

    DRAM DSE Setting - CK (ohm):            48

    DRAM DSE Setting - DQS (ohm):           48

    System ODT Setting (ohm):               60

I am not sure if all these values are ok.

After translating generated RealView.inc to mwh/mww phys instructions, I can initialize DDR3 memory via netcat:

    $ nc localhost 3333

    > ddr_init

After initializing RAM with register values generated by the aid tool, I am able to read/write single RAM addresses:

    > mww 0x10000000 0x1234567

    mww 0x10000000 0x1234567

    > mdw 0x10000000

    0x10000000: 01234567

After that, I try to load the stress test tool 'ddr-test-uboot-jtag-mx6dq.elf' into internal RAM memory:

    $ arm-none-eabi-gdb

    > target remote localhost:3333

    > load ddr_stress_tester_jtag_v2.52/ddr-test-uboot-jtag-mx6dq.elf

    > cont

Process completes wthout any output error, but I don't see anything on the debug console (configured at 115200, 8N1).

I will appreciate any help on this.

Thank you in advance!

标签 (1)
9 回复数

1,497 次查看
aicastell
Contributor II

Hello,

I have tried loading bin file as suggested, but I don't see any char written over UART1 console yet.

Attached are the steps I follow for your reference:

$ nc localhost 4444

> imx6d_init

imx6d_init

Call to imx6d_init...

number of cache level 1

imx6.cpu.0 cluster 0 core 0 multi core

target state: halted

target halted in Thumb state due to debug-request, current mode: Supervisor

cpsr: 0x600001f3 pc: 0x000024e4

MMU: disabled, D-Cache: disabled, I-Cache: disabled

Call to disable_wdog...

Call to imx6d_clock_init...

Call to imx6d_uart1_enable...

Call to imx6d_ddr3_1GB_init...

Ret from imx6d_init

> load_image ddr_stress_tester_v2.52/bin/ddr-test-mx6dq.bin 0x10000000

load_image ddr_stress_tester_v2.52/bin/ddr-test-mx6dq.bin 0x10000000

122016 bytes written at address 0x10000000

downloaded 122016 bytes in 76.891029s (1.550 KiB/s)

> step 0x10000000

step 0x10000000

target state: halted

target halted in Thumb state due to breakpoint, current mode: Supervisor

cpsr: 0x400001f3 pc: 0x10000002

MMU: disabled, D-Cache: disabled, I-Cache: disabled

> resume

resume

1,497 次查看
aicastell
Contributor II

Hello forum.

This issue is not fixed yet, I am still searching a solution for the described problem. It would be nice if some user with more experience on iMX.6 boards give some advice to try to discover what is wrong with this board.

Thank you in advance!

Best regards,

-- Ivan

1,497 次查看
engjoe
Contributor II

Also have this question, very similar set of steps but with the 6UL. No luck despite best efforts on UART register settings. 

DDR stress test via USB doesn't always work, so that isn't a good answer Yuri.

1,497 次查看
ivancastell
Contributor I

We still haven't found any useful information to solve this issue... Completely stalled with this board...

0 项奖励
回复

1,497 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Why do not use the DDR stress test, which is working via USB of i.MX6 ? 

Regards,

Yuri.

0 项奖励
回复

1,497 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Your (debug) configuration is not fully clear.  The DDR stress test is intended to work in
bare metal environment.


i.MX6/7 DDR Stress Test Tool V2.52

Please use internal (USB) boot ROM loader of i.MX6 or JTAG debugger.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,497 次查看
aicastell
Contributor II

Hello Mr. Yuri.

I am loading the elf stress test binary you point in your link (ddr_stress_tester_jtag_v2.52/ddr-test-uboot-jtag-mx6dq.elf) using a SEGGER J-Link PLUS JTAG with openocd (version 0.9.0). So I translate RealView.inc generated by xlsx document to openocd instructions (mww and mwh).

I can provide any missing parameter you require to try to solve this issue.

Thank you for your answer.

Best regards,

-- Ivan

1,497 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Can Your try to load and run memory image (.bin) file instead of .elf ?

Regards,

Yuri.

0 项奖励
回复

1,497 次查看
aicastell
Contributor II

Attached is the content of my openocd .cfg configuration file, so you can check all my control registers.

According to documentation, the DDR Stress Tester executable (starting with V2.20) has auto UART detection feature. Does this mean I don't have to setup any UART control register on my cfg file?.

Because after making different tests I don't see any output through the UART1, as a new test I tried adding a  "imx6d_uart1_enable" procedure to my .cfg file in order to setup UART1 manually. But still I don't see any character on the console.

Any help on this will be really helpful.

Thank you in advance!

telnet_port     4444

gdb_port        3333

source [find interface/jlink.cfg]

source [find target/imx6.cfg]

adapter_khz 50

jtag_ntrst_delay 50

$_TARGETNAME configure -event reset-start { adapter_khz 50 }

$_TARGETNAME configure -event reset-assert "imx6d_init"

proc imx6d_init {} {

    echo "Call to imx6d_init..."

  halt

    dap apcsw 1

    imx6d_wdog_disable

    imx6d_clock_init

    imx6d_uart1_enable

    imx6d_ddr3_1GB_init

    echo "Ret from imx6d_init"

}

proc imx6d_wdog_disable {} {

    echo "Call to disable_wdog..."

    set WDOG1_WCR 0x020bc000

    mwh phys $WDOG1_WCR 0x30

}

proc imx6d_clock_init {} {

   echo "Call to imx6d_clock_init..."

   set CCM_CCGR0 0x020c4068

   set CCM_CCGR1 0x020c406c

   set CCM_CCGR2 0x020c4070

   set CCM_CCGR3 0x020c4074

   set CCM_CCGR4 0x020c4078

   set CCM_CCGR5 0x020c407c

   set CCM_CCGR6 0x020c4080

   set CCM_CCGR7 0x020c4084

   # Enable all clocks

   mww phys $CCM_CCGR0 0xffffffff

   mww phys $CCM_CCGR1 0xffffffff

   mww phys $CCM_CCGR2 0xffffffff

   mww phys $CCM_CCGR3 0xffffffff

   mww phys $CCM_CCGR4 0xffffffff

   mww phys $CCM_CCGR5 0xffffffff

   mww phys $CCM_CCGR6 0xffffffff

   mww phys $CCM_CCGR7 0xffffffff

}

proc imx6d_uart1_enable {} {

    echo "Call to imx6d_uart1_enable..."

    set UART1_UCR1 0x02020080

    set UART1_UCR2 0x02020084

    set UART1_UCR3 0x02020088

    set UART1_UCR4 0x0202008C

    set UART1_URXD 0x02020000

    set UART1_UTXD 0x02020040

    set UART2_UCR1 0x021E8080

    set UART2_UCR2 0x021E8084

    set UART2_UCR3 0x021E8088

    set UART2_UCR4 0x021E808C

    set UART2_URXD 0x021E8000

    set UART2_UTXD 0x021E8040

    set UART3_UCR1 0x021EC080

    set UART3_UCR2 0x021EC084

    set UART3_UCR3 0x021EC088

    set UART3_UCR4 0x021EC08C

    set UART3_URXD 0x021EC000

    set UART3_UTXD 0x021EC040

    set UART4_UCR1 0x021F0080

    set UART4_UCR2 0x021F0084

    set UART4_UCR3 0x021F0088

    set UART4_UCR4 0x021F008C

    set UART4_URXD 0x021F0000

    set UART4_UTXD 0x021F0040

    # Enable UART1, data = 8bits

    mww phys $UART1_UCR1 0x00000001

    mww phys $UART1_UCR2 0x00000026

}

proc imx6d_ddr3_1GB_init {} {

    echo "Call to imx6d_ddr3_1GB_init..."

    set MX6_IOM_DRAM_DQM0       0x020e05ac

    set MX6_IOM_DRAM_DQM1       0x020e05b4

    set MX6_IOM_DRAM_DQM2       0x020e0528

    set MX6_IOM_DRAM_DQM3       0x020e0520

    set MX6_IOM_DRAM_DQM4       0x020e0514

    set MX6_IOM_DRAM_DQM5       0x020e0510

    set MX6_IOM_DRAM_DQM6       0x020e05bc

    set MX6_IOM_DRAM_DQM7       0x020e05c4

    set MX6_IOM_DRAM_CAS        0x020e056c

    set MX6_IOM_DRAM_RAS        0x020e0578

    set MX6_IOM_DRAM_RESET      0x020e057c

    set MX6_IOM_DRAM_SDCLK_0    0x020e0588

    set MX6_IOM_DRAM_SDCLK_1    0x020e0594

    set MX6_IOM_DRAM_SDBA2      0x020e058c

    set MX6_IOM_DRAM_SDCKE0     0x020e0590

    set MX6_IOM_DRAM_SDCKE1     0x020e0598

    set MX6_IOM_DRAM_SDODT0     0x020e059c

    set MX6_IOM_DRAM_SDODT1     0x020e05a0

    set MX6_IOM_DRAM_SDQS0      0x020e05a8

    set MX6_IOM_DRAM_SDQS1      0x020e05b0

    set MX6_IOM_DRAM_SDQS2      0x020e0524

    set MX6_IOM_DRAM_SDQS3      0x020e051c

    set MX6_IOM_DRAM_SDQS4      0x020e0518

    set MX6_IOM_DRAM_SDQS5      0x020e050c

    set MX6_IOM_DRAM_SDQS6      0x020e05b8

    set MX6_IOM_DRAM_SDQS7      0x020e05c0

    set MX6_IOM_GRP_B0DS        0x020e0784

    set MX6_IOM_GRP_B1DS        0x020e0788

    set MX6_IOM_GRP_B2DS        0x020e0794

    set MX6_IOM_GRP_B3DS        0x020e079c

    set MX6_IOM_GRP_B4DS        0x020e07a0

    set MX6_IOM_GRP_B5DS        0x020e07a4

    set MX6_IOM_GRP_B6DS        0x020e07a8

    set MX6_IOM_GRP_B7DS        0x020e0748

    set MX6_IOM_GRP_ADDDS       0x020e074c

    set MX6_IOM_DDRMODE_CTL     0x020e0750

    set MX6_IOM_GRP_DDRPKE      0x020e0758

    set MX6_IOM_GRP_DDRMODE     0x020e0774

    set MX6_IOM_GRP_CTLDS       0x020e078c

    set MX6_IOM_GRP_DDR_TYPE    0x020e0798

    set MX6_MMDC_P0_MDCTL       0x021b0000

    set MX6_MMDC_P0_MDPDC       0x021b0004

    set MX6_MMDC_P0_MDOTC       0x021b0008

    set MX6_MMDC_P0_MDCFG0      0x021b000c

    set MX6_MMDC_P0_MDCFG1      0x021b0010

    set MX6_MMDC_P0_MDCFG2      0x021b0014

    set MX6_MMDC_P0_MDMISC      0x021b0018

    set MX6_MMDC_P0_MDSCR       0x021b001c

    set MX6_MMDC_P0_MDREF       0x021b0020

    set MX6_MMDC_P0_MDRWD       0x021b002c

    set MX6_MMDC_P0_MDOR        0x021b0030

    set MX6_MMDC_P0_MDASP       0x021b0040

    set MX6_MMDC_P0_MAPSR       0x021b0404

    set MX6_MMDC_P0_MPZQHWCTRL  0x021b0800

    set MX6_MMDC_P0_MPWLDECTRL0 0x021b080c

    set MX6_MMDC_P0_MPWLDECTRL1 0x021b0810

    set MX6_MMDC_P0_MPODTCTRL   0x021b0818

    set MX6_MMDC_P0_MPRDDQBY0DL 0x021b081c

    set MX6_MMDC_P0_MPRDDQBY1DL 0x021b0820

    set MX6_MMDC_P0_MPRDDQBY2DL 0x021b0824

    set MX6_MMDC_P0_MPRDDQBY3DL 0x021b0828

    set MX6_MMDC_P0_MPDGCTRL0   0x021b083c

    set MX6_MMDC_P0_MPDGCTRL1   0x021b0840

    set MX6_MMDC_P0_MPRDDLCTL   0x021b0848

    set MX6_MMDC_P0_MPWRDLCTL   0x021b0850

    set MX6_MMDC_P0_MPMUR0      0x021b08b8

    set MX6_MMDC_P1_MDCTL       0x021b4000

    set MX6_MMDC_P1_MDPDC       0x021b4004

    set MX6_MMDC_P1_MDOTC       0x021b4008

    set MX6_MMDC_P1_MDCFG0      0x021b400c

    set MX6_MMDC_P1_MDCFG1      0x021b4010

    set MX6_MMDC_P1_MDCFG2      0x021b4014

    set MX6_MMDC_P1_MDMISC      0x021b4018

    set MX6_MMDC_P1_MDSCR       0x021b401c

    set MX6_MMDC_P1_MDREF       0x021b4020

    set MX6_MMDC_P1_MDRWD       0x021b402c

    set MX6_MMDC_P1_MDOR        0x021b4030

    set MX6_MMDC_P1_MDASP       0x021b4040

    set MX6_MMDC_P1_MAPSR       0x021b4404

    set MX6_MMDC_P1_MPZQHWCTRL  0x021b4800

    set MX6_MMDC_P1_MPWLDECTRL0 0x021b480c

    set MX6_MMDC_P1_MPWLDECTRL1 0x021b4810

    set MX6_MMDC_P1_MPODTCTRL   0x021b4818

    set MX6_MMDC_P1_MPRDDQBY0DL 0x021b481c

    set MX6_MMDC_P1_MPRDDQBY1DL 0x021b4820

    set MX6_MMDC_P1_MPRDDQBY2DL 0x021b4824

    set MX6_MMDC_P1_MPRDDQBY3DL 0x021b4828

    set MX6_MMDC_P1_MPDGCTRL0   0x021b483c

    set MX6_MMDC_P1_MPDGCTRL1   0x021b4840

    set MX6_MMDC_P1_MPRDDLCTL   0x021b4848

    set MX6_MMDC_P1_MPWRDLCTL   0x021b4850

    set MX6_MMDC_P1_MPMUR0      0x021b48b8

    #===========================================================================

    # IOMUX

    #===========================================================================

    # DDR IO type

    mww phys  $MX6_IOM_GRP_DDR_TYPE     0x000C0000

    mww phys  $MX6_IOM_GRP_DDRPKE       0x00000000

    # Clock

    mww phys  $MX6_IOM_DRAM_SDCLK_0     0x00000028

    mww phys  $MX6_IOM_DRAM_SDCLK_1     0x00000028

    # Address

    mww phys  $MX6_IOM_DRAM_CAS         0x00000028

    mww phys  $MX6_IOM_DRAM_RAS         0x00000028

    mww phys  $MX6_IOM_GRP_ADDDS        0x00000028

    # Control

    mww phys  $MX6_IOM_DRAM_RESET       0x00000028

    mww phys  $MX6_IOM_DRAM_SDBA2       0x00000000

    mww phys  $MX6_IOM_DRAM_SDODT0      0x00000028

    mww phys  $MX6_IOM_DRAM_SDODT1      0x00000028

    mww phys  $MX6_IOM_GRP_CTLDS        0x00000028

    # Data Strobes

    mww phys  $MX6_IOM_DDRMODE_CTL      0x00020000

    mww phys  $MX6_IOM_DRAM_SDQS0       0x00000028

    mww phys  $MX6_IOM_DRAM_SDQS1       0x00000028

    mww phys  $MX6_IOM_DRAM_SDQS2       0x00000028

    mww phys  $MX6_IOM_DRAM_SDQS3       0x00000028

    # mww phys $MX6_IOM_DRAM_SDQS4      0x00000028

    # mww phys $MX6_IOM_DRAM_SDQS5      0x00000028

    # mww phys $MX6_IOM_DRAM_SDQS6      0x00000028

    # mww phys $MX6_IOM_DRAM_SDQS7      0x00000028

    # Data

    mww phys  $MX6_IOM_GRP_DDRMODE      0x00020000

    mww phys  $MX6_IOM_GRP_B0DS         0x00000028

    mww phys  $MX6_IOM_GRP_B1DS         0x00000028

    mww phys  $MX6_IOM_GRP_B2DS         0x00000028

    mww phys  $MX6_IOM_GRP_B3DS         0x00000028

    # mww phys $MX6_IOM_GRP_B4DS        0x00000028

    # mww phys $MX6_IOM_GRP_B5DS        0x00000028

    # mww phys $MX6_IOM_GRP_B6DS        0x00000028

    # mww phys $MX6_IOM_GRP_B7DS        0x00000028

    mww phys  $MX6_IOM_DRAM_DQM0        0x00000028

    mww phys  $MX6_IOM_DRAM_DQM1        0x00000028

    mww phys  $MX6_IOM_DRAM_DQM2        0x00000028

    mww phys  $MX6_IOM_DRAM_DQM3        0x00000028

    # mww phys $MX6_IOM_DRAM_DQM4       0x00000028

    # mww phys $MX6_IOM_DRAM_DQM5       0x00000028

    # mww phys $MX6_IOM_DRAM_DQM6       0x00000028

    # mww phys $MX6_IOM_DRAM_DQM7       0x00000028

    mww phys  $MX6_MMDC_P0_MDSCR        0x00008000

    #===========================================================================

    # Calibration setup.

    #===========================================================================

    mww phys  $MX6_MMDC_P0_MPZQHWCTRL   0xA1390003

    # For target board, may need to run write leveling calibration to fine tune these settings.

    mww phys  $MX6_MMDC_P0_MPWLDECTRL0  0x00000000

    mww phys  $MX6_MMDC_P0_MPWLDECTRL1  0x00000000

    ## Read DQS Gating calibration

    mww phys  $MX6_MMDC_P0_MPDGCTRL0    0x00000000

    mww phys  $MX6_MMDC_P0_MPDGCTRL1    0x00000000

    # Read calibration

    mww phys  $MX6_MMDC_P0_MPRDDLCTL    0x40404040

    # Write calibration

    mww phys  $MX6_MMDC_P0_MPWRDLCTL    0x40404040

    # Read data bit delay: (3 is the recommended default value, although out of reset value is 0)

    mww phys  $MX6_MMDC_P0_MPRDDQBY0DL  0x33333333

    mww phys  $MX6_MMDC_P0_MPRDDQBY1DL  0x33333333

    mww phys  $MX6_MMDC_P0_MPRDDQBY2DL  0x33333333

    mww phys  $MX6_MMDC_P0_MPRDDQBY3DL  0x33333333

    # mww phys $MX6_MMDC_P1_MPRDDQBY0DL 0x33333333

    # mww phys $MX6_MMDC_P1_MPRDDQBY1DL 0x33333333

    # mww phys $MX6_MMDC_P1_MPRDDQBY2DL 0x33333333

    # mww phys $MX6_MMDC_P1_MPRDDQBY3DL 0x33333333

    # Complete calibration by forced measurement

    mww phys  $MX6_MMDC_P0_MPMUR0       0x00000800

    # MMDC init

    mww phys  $MX6_MMDC_P0_MDPDC        0x0002002D

    mww phys  $MX6_MMDC_P0_MDOTC        0x00333040

    mww phys  $MX6_MMDC_P0_MDCFG0       0x2B2F5333

    mww phys  $MX6_MMDC_P0_MDCFG1       0xB5EB8B63

    mww phys  $MX6_MMDC_P0_MDCFG2       0x01FF00DB

    mww phys  $MX6_MMDC_P0_MDMISC       0x00011740

    mww phys  $MX6_MMDC_P0_MDSCR        0x00008000

    mww phys  $MX6_MMDC_P0_MDRWD        0x000026D2

    mww phys  $MX6_MMDC_P0_MDOR         0x002F1023

    mww phys  $MX6_MMDC_P0_MDASP        0x0000000F

    mww phys  $MX6_MMDC_P0_MDCTL        0x84190000

    # Mode register writes

    mww phys  $MX6_MMDC_P0_MDSCR        0x02008032

    mww phys  $MX6_MMDC_P0_MDSCR        0x00008033

    mww phys  $MX6_MMDC_P0_MDSCR        0x00048031

    mww phys  $MX6_MMDC_P0_MDSCR        0x15208030

    mww phys  $MX6_MMDC_P0_MDSCR        0x04008040

    mww phys  $MX6_MMDC_P0_MDREF        0x00007800

    mww phys  $MX6_MMDC_P0_MPODTCTRL    0x00022227

    mww phys  $MX6_MMDC_P0_MDPDC        0x0002556D

    mww phys  $MX6_MMDC_P0_MAPSR        0x00011006

    mww phys  $MX6_MMDC_P0_MDSCR        0x00000000

}

0 项奖励
回复