hello,
I am using SkHynix H5TC2G63GFR-PBI DDR3 on imx6ull, there is some question about DDR3 Porting, Is there someone can help me? thanks first.
Q1: Is there a special DDR3_Script_Aid tools for imx6ull? I have download a imx6ul aid that the name is <I.MX6UL_DDR3_Script_Aid_V0.02.xlsx> from this community
https://community.nxp.com/docs/DOC-329899
. is this ok?
Q2: how to setup DDR3_Script_Aid? there are some item which I have no idea.
Device Information | |||
Manufacturer: | Micron | SKhynix | |
Memory part number: | MT41K256M16HA-125 | H5TC2G63GFR-PBI | |
Memory type: | DDR3-1600 | DDR3-1600 | |
DRAM density (Gb) | 4 | 2 | |
DRAM Bus Width | 16 | 16 | |
Number of Banks | 8 | 8 | |
Number of ROW Addresses | 15 | 14 | |
Number of COLUMN Addresses | 10 | 10 | |
Page Size (K) | 2 | 2 | |
Self-Refresh Temperature (SRT) | Extended | Extended | |
CAS READ latency (CL) | 8 | ? | Programmable CAS latency 6, 7, 8, 9, 10, 11, 12 and 13 supported |
tRCD=tRP=CL (ns) | 13.75 | ? | |
tRC Min (ns) | 48.75 | 50.625 | |
tRAS Min (ns) | 35 | 37.5 | |
System Information | |||
i.Mx Part | i.MX6UL | iMX6ULL | |
Bus Width | 16 | 16 | |
Density per chip select (Gb) | 4 | 2 | |
Number of Chip Selects used | 1 | 1 | |
Total DRAM Density (Gb) | 4 | 2 | |
DRAM Clock Freq (MHz) | 400 | 400 | |
DRAM Clock Cycle Time (ns) | 2.5 | 1.25? | |
Address Mirror (for CS1) | Disable | Disable | |
SI Configuration | |||
DRAM DSE Setting - DQ/DQM (ohm) | 48 | 48 | |
DRAM DSE Setting - ADDR/CMD/CTL (ohm) | 48 | 48 | |
DRAM DSE Setting - CK (ohm) | 48 | 48 | |
DRAM DSE Setting - DQS (ohm) | 48 | 48 | |
System ODT Setting (ohm) | 60 | 60 |
Q3: the last one about NXP DDR Test tool , What is the Value about MR1 Values(Hex)?
已解决! 转到解答。
Hello,
Customers can use the following tool:
“i.MX6ULL_DDR3_Script_Aid”
https://community.nxp.com/docs/DOC-333791
MR1 value should be the same as in the initialization script.
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.