DDR3 Bit Swaaping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR3 Bit Swaaping

Jump to solution
1,252 Views
muralikrishna
Contributor I

We swapped the DDR3 bits as recommended.

How to map these bits to processor while initializing.

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
1,069 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
5 Replies
1,070 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
1,069 Views
art
NXP Employee
NXP Employee

Also, when swapping the byte lanes, don't forget to route correctly the strobe and mask signals, i.e. DQMx, DQSx and DQSx_B, corresponding to these byte lanes.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,069 Views
igorpadykov
NXP Employee
NXP Employee

Hi Murali

there is no need for additional mapping or software reconfiguration, as

it is done automatically. Bit swapping is described in sect.3.5.1 Swapping data lines IMX6DQ6SDLHDG also

below part of p.4 SPF-27392 Sabre Schematic i.MX6_SABRE_SDP_DESIGNFILES :

SPF-27392   p.4.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,069 Views
muralikrishna
Contributor I

Hi igor,

Bit swapping in Hardware is taken care.

How to implement those bit swappings in software to write or read to DDR3

Murali

0 Kudos
Reply
1,069 Views
igorpadykov
NXP Employee
NXP Employee

Hi Murali

in general it is not possible to implement bit swappings in software.

If you followed Freescale recommmendations, there is no need

for additional mapping or software reconfiguration,

Best regards

igor

0 Kudos
Reply