I use Mx6DQSDL DDR3 Script Aid V0.08 and DDR stress tester v1.0.2 to calibrate i.MX6DL board DDR3.
prj00119-imx6dl-ddr3.inc
MX6DL opened.
HAB_TYPE: DEVELOP
rom_write: reading HAB ack failed 0x00000000
ROM Write failed, addr: 0x021b001c
Write dcd failed.
If I just keep the first line of 0x021b001c access and comment out others, the test can go on, but still hang after setting DDR frequency as below.
prj00119-imx6dl-ddr3-2.inc
MX6DL opened.
HAB_TYPE: DEVELOP
Image loading...
download Image to IRAM OK
Re-open MX6x device.
Running DDR test..., press "ESC" key to exit.
******************************
DDR Stress Test (1.0.2) for MX6DL
Build: Dec 10 2013, 12:31:47
Freescale Semiconductor, Inc.
******************************
=======DDR configuration==========
BOOT_CFG3[5-4]: 0x00, Single DDR channel.
DDR type is DDR3
Data width: 64, bank num: 8
Row size: 14, col size: 10
Chip select CSD0 is used
Density per chip select: 1024MB
==================================
What ARM core speed would you like to run?
Type 0 for 650MHz, 1 for 800MHz, 2 for 1GHz
ARM set to 1GHz
Please select the DDR density per chip select (in bytes) on the board
Type 0 for 2GB; 1 for 1GB; 2 for 512MB; 3 for 256MB; 4 for 128MB; 5 for 64MB; 6
for 32MB
For maximum supported density (4GB), we can only access up to 3.75GB. Type 9 to
select this
DDR density selected (MB): 1024
Calibration will run at DDR frequency 400MHz. Type 'y' to continue.
If you want to run at other DDR frequency. Type 'n'
Original Attachment has been moved to: prj00119-imx6dl-ddr3-2.inc.zip
Original Attachment has been moved to: prj00119-imx6dl-ddr3.inc.zip
Solved! Go to Solution.
Probably smth wrong with hardware, try SDK (ddr_test.c), verify
that it does not hang. Run it with jtag, check power, DDR signals with oscilloscope
"MX6_PLATFORM_SDK "
Probably smth wrong with hardware, try SDK (ddr_test.c), verify
that it does not hang. Run it with jtag, check power, DDR signals with oscilloscope
"MX6_PLATFORM_SDK "
It's hardware issue because didn't happend on the other board.