Goodmorning i.MX community,
I have a question regarding the differences of the DDR stress-test tools version 1.03 and 2.60. It seems that the 2.60 stress test is more strict or faster that the 1.03 test. Please note that I only use the stress test part of the tool and skip the calibration process to compare both tools.
I have here a board that was calibrated with the 1.03 tool and the stress test passed for > 100 times. When I run the stress test 2.60 it fails in the first or second run...
Can somebody confirm that the the 2.60 tool stress testing is improved / faster than 1.03? What are the differences?
Best regards, Pieter
解決済! 解決策の投稿を見る。
Hi Pieter
you are right, v2.60 is faster compared to v1.03 as it enables cache.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Pieter
you are right, v2.60 is faster compared to v1.03 as it enables cache.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------