DDR Stress Test in IMX8QM Custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress Test in IMX8QM Custom board

894 Views
vinothkumars
Senior Contributor IV

Hello,

Software/ Hardware details,

L4.14.98 + IMX8QM Custom Board

SCFW 1.2.1

RPA: V17

ER8

 

I got the following response from DDR Stress Test,

 

 

If you want to watch DDR script executing process, please open SCU debug uart in other serial tool

Waiting for the target board boot...

 

 

Regards,
Vinothkumar Sekar
0 Kudos
4 Replies

884 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

reason for that behaviour may wrongly configured uart, one can look at below link  "FAQs:"

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8-8X-Family-DDR-Tools-Release/ta-p/...

Also recommended to attach another terminal to " SCU debug uart" as suggests ddr test log.

 

Best regards
igor

0 Kudos

873 Views
vinothkumars
Senior Contributor IV

Thank you @igorpadykov for the reply.

 

Also recommended to attach another terminal to " SCU debug uart" as suggests ddr test log.

<Vinoth> Currently there is one debug UART in custom board. Is it enough to do the DDR Stress Test ?

 

failed.png

 

 

Regards,
Vinothkumar Sekar
0 Kudos

864 Views
igorpadykov
NXP Employee
NXP Employee

for " SCU debug uart" please refer to documentation included in  SCFW Porting Kit​

 

Best regards
igor

 

0 Kudos

849 Views
vinothkumars
Senior Contributor IV

Hi @igorpadykov 

 

 

My custom board hanged here, I unable to find out the any log due to one debug uart in custom board by default.


i.MX8QM_B0 is found
Download is complete£¡
If you want to watch DDR script executing proces, please open SCU debug uart in other serial tool
Waiting for the target board boot...


I got the following log from DDR Stress Test Tool. But, the hardware is limited to one debug uart (UART1).


Is it possible to enable/route all message through one debug UART ?.

Will you please provide the SCFW board configuration file (with modified debug uart) for UART1 for SCU UART.

or Do I needs to do any hardware modification ?

 

 

 

Regards,
Vinothkumar Sekar
0 Kudos