DDR Stress Test failed for IMX8QM Custom Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress Test failed for IMX8QM Custom Board

Jump to solution
2,325 Views
vinothkumars
Senior Contributor IV

Dear NXP,

 

DDR stress test failed. Will you please give some idea regarding the following errors,

 

*************************************************************************
MX8 DDR Stress Test Version: ER14
Built on Mar 27 2020 12:19:30
*************************************************************************

--Set up the MMU and enable I and D cache--
- This is the Cortex-A72 core
Adjusting CA72 cache latency
- Check if I cache is enabled
- Enabling I cache since it was disabled
- Push base address of TTB to TTBR0_EL3
- Config TCR_EL3
- Config MAIR_EL3
- Enable MMU
- Data Cache has been enabled
- Check system memory register, only for debug

- VMCR Check:
- ttbr0_el3: 0x13d000
- tcr_el3: 0x2051c
- mair_el3: 0x774400
- sctlr_el3: 0xc01815
- id_aa64mmfr0_el1: 0x1124

- MMU and cache setup complete

*************************************************************************
ARM Clock(CA72): 1596MHz
DDR Clock: 1596MHz

============================================
DDR configuration
DDR type is LPDDR4
Data width: 32, bank num: 8
Row size: 15, col size: 10
Two chip selects are used
Number of DDR controllers used on the SoC: 2
Density per chip select: 1024MB
Density per controller is: 2048MB
Total density detected on the board is: 4096MB

Note: As this SoC has more than one DDR Controller, the calculated
density assumes all controllers are being used. Adjust the tested
density per your board configuration if not all controllers are used

 

********************************************
WARNING! DDR training errors were detected on DDRC 0!
DDR_PHY_PGSR0 = 0x806cc07f
DQS Gate training error detected
Write Leveling training error detected
VREF training error detected
Write DQS2DQ training error detected
Recheck DDR initialization
********************************************


********************************************
WARNING! DDR training errors were detected on DDRC 1!
DDR_PHY_PGSR0 = 0x806cc07f
DQS Gate training error detected
Write Leveling training error detected
VREF training error detected
Write DQS2DQ training error detected
Recheck DDR initialization
********************************************
============================================

MX8QM: Cortex-A72 is found

*************************************************************************

 

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
1 Solution
2,277 Views
igorpadykov
NXP Employee
NXP Employee

I believe Chan B is configured incorrectly. For example:
on your schematic DQ0_B (pad AA2) is connected to DDR0_B_DQ4 (DDR_CH0_DQ20)
so Excel "BoardDataBusConfig" Chan B should be:
DRAM Data bus 0
MX8QM data bus (User Input)-> 20

DQ1_B (pad Y2) is connected to DDR0_B_DQ7 (DDR_CH0_DQ23)

so Excel "BoardDataBusConfig" should be:
DRAM Data bus 1
MX8QM data bus (User Input)-> 23

e.t.c.

 

Best regards
igor

 

 

View solution in original post

0 Kudos
Reply
3 Replies
2,305 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vinothkumar

 

reason for this issue may be wrong memory connections or incorrectly configured "BoardDataBusConfig"

parameters in RPA tool.

 

Best regards
igor

0 Kudos
Reply
2,295 Views
vinothkumars
Senior Contributor IV

Thank you @igorpadykov  for the reply.

 

Will you please validate my BoardDataBusConfig section for DDRC0.

 

 

DDRC0.png

DDRC0_1.png

  

 

Regards,
Vinothkumar Sekar
0 Kudos
Reply
2,278 Views
igorpadykov
NXP Employee
NXP Employee

I believe Chan B is configured incorrectly. For example:
on your schematic DQ0_B (pad AA2) is connected to DDR0_B_DQ4 (DDR_CH0_DQ20)
so Excel "BoardDataBusConfig" Chan B should be:
DRAM Data bus 0
MX8QM data bus (User Input)-> 20

DQ1_B (pad Y2) is connected to DDR0_B_DQ7 (DDR_CH0_DQ23)

so Excel "BoardDataBusConfig" should be:
DRAM Data bus 1
MX8QM data bus (User Input)-> 23

e.t.c.

 

Best regards
igor

 

 

0 Kudos
Reply