I would like to use the "DDR STRESS TEST" program as the Command Line.
The product is connected by USB.
I understand that USB options are supported through the GUI.
Is there any way I can use it through Windows Command Line?
Hi Igor,
We too have a requirement to use DDR stress tool from command line with iMx8QXP.
Whether ddr_stress_tester_uboot_vX.xx.zip (Option 3 uboot) or similar tool available for iMx8X ?
Regards,
Krishna
Hi jaehoon
available options are provided on i.MX6/7 DDR Stress Test Tool V3.00
seems there is no command line option, probably one can consider "Option 3 U-Boot".
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------