DCDC_BATT and VDD4P2 connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DCDC_BATT and VDD4P2 connection

529 次查看
semihhazar
Contributor II

Hi,

We're using imx28 in 4V input only scenario and supplying power to DCDC_BATT and BATTERY pins. Since VDD5V is not used, 4P2LinReg is not used and I assume there's no use of the VDD4P2 pin. But why is there a diode connecting DCDC_BATT to VDD4P2?

I'd appreciate if you could briefly explain this.

Regards,

Semih

标签 (1)
0 项奖励
1 回复

377 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Semih

the purpose of the diode to guarantee the supply to the DCDC is not

interrupted when switching from battery to VDD4P2.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励