Custom IMX8MM Board's DDR3L DS Config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Custom IMX8MM Board's DDR3L DS Config

1,519 Views
houssem_chaaban
Contributor II

Hello all,

We made a custom board based on iMX8MM chip, with DDR3L RAM.

We are using Yocto project to build an compatible image for the DDR3L : imx8mmddr3lval

Yocto provides a ready imx-boot to flash the eMMC with as well as the built image.

But Yocto by default generate the bootloader with the default evalboard ddr3_timing.c file.

We know that we have to use the DDR Stress Test Tool provided by NXP in order to generate a new custom ddr3_timing.c file for the bootloader.

_______________[ Here's some screenshots problems we've faced ]_______________

1. Training ERROR while flashing with default bootloader

We tried to modify the DS file as possible as we can understand and we pass the Calibration but not the Stress test.

2. The new ERROR with the new ddr3_timing.c file

__________________________________________________________________

So, for that purpose, we need to generate a new DS file for that tool as guided here : iMX8-MSCALE

But we do not know how exactly that could be done with its many DDR technical details which we do not have a knowledge on.

So we attached with post two documents as follow:

  • Data sheet of our DDR
  • The DDR Stress Tool excel file

So basically our need is to fill in correctly the fields of the DDR tool excel file in order to:

  • Generate a correct DS file for our board
  • Pass the Calibration and Stress tests correctly
  • Generate a valid ddr3_timing.c file
  • Rebuild u-boot to be able to flash the eMMC

_______

THANK YOU !

1 Reply

1,216 Views
houssem_chaaban
Contributor II

Hello all,

This is an update for this issue:

We tried to fill the excel file again with more details from the datasheet of our DDR.

And now the calibration and the Stress test pass good.

Best Regards.