Hi,@igorpadykov
We have designed custom Board based on i.mx8quadmax - MEK Evaluation board.
It boots -u-boot and working fine.
When it loads the Linux kernel at the near to end of login scripts it crashes.
Almost when it starts the services , it crashes(i.mx media image kernel). randomly different points.
Status:
1) It Passes the DDR Stress Test.
2) Build Root Linux kernel is working fine.
3) Yocto - minimal image also crashing.
But, If disable services in yocto packages itself, it is working fine.
4) Sometime 10 out of 1 it boots properly without issue.
What could be the problem?
Pls suggest.
Reports attached here
1) Kernel crash report
2) DDR Stress test report
Regards
Ramesh
Pleasure to Interact With you
1) Null Pointer Issue.
This bug is taken care in Kernel 5.15.32 as per the way you suggested.We have tested our board with kernel 5.15.32. The issue is appeared again. crashing..!!!
We have tested the Board with kernel 5.15.32 - Core Minimal Image with systemd completely removed.
Then , It Boots every time.
Then , We ran the parallel memory bandwidth test.
https://community.nxp.com/t5/i-MX-Processors/Memory-Bandwidth-Measurement-Tool/m-p/989913
It starts loading the Memory slowly by increasing the thread count and Buffer size.
Like Thread count : 1,2,3..along with buffer size.
It crashes every time when the thread count becomes 3.
Hence , LPDDR4 bandwidth issue / DDR4 memory timing issue - identified.
Whether it is due to board fabrication OR DDR4 memory part issue
Pls suggest further
Regards
Ramesh
Hi @RameshChandrakasan ,