Crsyatl and Oscillator for i.MX6UL

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Crsyatl and Oscillator for i.MX6UL

441 次查看
surendrajadhav
Contributor IV

Hello,

I was referring to EVK of i.MX6UL. However I could not not get the part numbers of crystal and Oscillator used on EVK.

Can anyone share me the part numbers of both.

Thanks,

Surendra

标签 (1)
0 项奖励
3 回复数

346 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Please use BOM file in design files package :

http://www.nxp.com/assets/downloads/data/en/schematics/MCIMX6UL-EVK_DESIGNFILES.zip 

Summary page :

i.MX6UltraLite Evaluation Kit|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励

346 次查看
surendrajadhav
Contributor IV

After going through EVK of NXP I founf two resistors are added at the output of Oscillator.

I think they may be used to downconvert the 3.3V output to 1.1V(NVCC_PLL).

Same is shown with red circles in the attached image.

Let me know your inputs on this.

 

Regards,

Surendra.i.MX6L Oscillator.png

0 项奖励

346 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The i.MX6 UL TO 1.0 (Maskset ID:0N52P) has some issues. Please use the TO 1.1 (Maskset ID: 1N52P).

For this release the recent Hardware Development Guide for the i.MX 6UltraLite should be used.

 

http://www.nxp.com/assets/documents/data/en/user-guides/IMX6ULHDG.pdf 

 

Please refer to 2.6 (Migrating from i.MX 6UltraLite TO1.0 to TO1.1).

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励