Hi everybody,I need to build Opencv2.2 for LTIB.I found it in FTF_CON_F0321_OpenCVontheimx53QuickStartBoard.pdf by eric gregori but it's not cleary.Can anyone else help me this problem?.I have been search all topic on imxcommunity,but it have no result.
I found some information in this document:
At slide 69,70,71,there're some guides to Cross compile Opencv2.2 for imx53 QSB LTIB,but it's not cleary.imxcommunity.org changed there interface,so that I could't find what Eric Gregori said in slide 70.
I have been search all disscusion in IMX53 QSB topic but i'm still stuck in this.
Please help me in this problem,thank you so much.
Take a look to this post
Re: Missing Content "Cross Compiling Opencv2.2 for I.MX53 QSB"
This might help to solve your issue.
Thanks Francisco Alberto Carrillo Dominguez,I have been try this so many time.But It doesn't work.It cross about 58% when i run "make",there're an error in module high gui,i think.
Ohhhh yeahhhh....Thank you so much Francisco,thank you!!!....From the bottom of my heart.
Please follow the guide that i posted, if you do everything as said there it will fail as you said at 58% with the following error:
Building CXX object modules/ml/CMakeFiles/opencv_ml.dir/src/gbt.o
/home/windows/Downloads/OpenCV-2.2.0/modules/ml/src/gbt.cpp: In member function 'virtual void CvGBTrees::find_gradient(int)':
/home/windows/Downloads/OpenCV-2.2.0/modules/ml/src/gbt.cpp:474: error: 'expl' was not declared in this scope
make[2]: *** [modules/ml/CMakeFiles/opencv_ml.dir/src/gbt.o] Error 1
make[1]: *** [modules/ml/CMakeFiles/opencv_ml.dir/all] Error 2
make: *** [all] Error 2
windows@ubuntu:~/Downloads/OpenCV-2.2.0$
This can be fixed with the following modification:
> Change line 14 ofOpenCV-2.2.0/modules/ml/src/gbt.cppfrom "Android" to "1"
- before -
#if Android
#define expl(x) exp(x)
#endif
- after -
#if 1
#define expl(x) exp(x)
#endif
With this Change it should work for 100%
Good luck!!
Francisco
Hi Francisco.Thank you very much for your help,but I saw this errors in highgui at 58%.
pp:49:27: error: dc1394/dc1394.h: No such file or directory
/home/lucid/OpenCV22_CrossBuild/OpenCV-2.2.0/modules/highgui/src/cap_dc1394_v2.cpp:53: error: 'dc1394error_t' does not name a type
/home/lucid/OpenCV22_CrossBuild/OpenCV-2.2.0/modules/highgui/src/cap_dc1394_v2.cpp:126: error: 'dc1394error_t' does not name a type
/home/lucid/OpenCV22_CrossBuild/OpenCV-2.2.0/modules/highgui/src/cap_dc1394_v2.cpp:157: error: 'dc1394camera_t' was not declared in this scope
/home/lucid/OpenCV22_CrossBuild/OpenCV-2.2.0/modules/highgui/src/cap_dc1394_v2.cpp:157: error: 'camera' was not declared in this scope
I guess because I'm missing 2 patch. An error occurred when I try to down 2 patch from the link
Can you attach two patch used to build opencv for arm.Thank you so much.:D.
This looks different, the patch will not fix your error.
I think you have other problem. What is your CMAKE line you are using?
This is CMAKE line i used:
cmake -DCMAKE_BUILD_TYPE=RELEASE -DCMAKE_INSTALL_PREFIX=/home/lucid/ltib/rootfs/usr/ -DCMAKE_TOOLCHAIN_FILE:PATH=${PWD}/../imx53.cmake -DCMAKE_FIND_ROOT_PATH=/home/lucid/ltib/rootfs/ -DWITH_FFMPEG=OFF -DWITH_GSTREAMER=OFF -DWITH_PYTHON=OFF -DWITH_GTK=OFF -DBUILD_EXAMPLES=ON ..
Where can i put imx53.cmake file.Do i need to modify this file.An error occurred when systems build highgui lib i think.