Could not download the cst-hsm.git

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Could not download the cst-hsm.git

629 次查看
AlpinaInformatik
Contributor I

Dear Community,

I am trying to download the cst-hsm repository and it is not working.

--Cmd: git clone ssh://git@bitbucket.sw.nxp.com/micrse/cst-hsm.git

--Error: Cloning into 'cst-hsm'...
ssh: connect to host bitbucket.sw.nxp.com port 22: Connection refused
fatal: Could not read from remote repository.

Please make sure you have the correct access rights
and the repository exists.

 

-- Where can I get the repository?

 

Kind Regards

Alpina Informatik

0 项奖励
回复
1 回复

611 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi @AlpinaInformatik 

You can get it from CST TOOL. IMX_CST_TOOL_NEW (nxp.com). But cst-hsm is a part of the cst tool source code, you need to compare it.

Best regards

Harvey

0 项奖励
回复