Hi all,
we are using on a custom board an imx6dp with isl79987 chip.
We are based on yocto warrior fsl release (kernel 4.19, yocto warrior).
i have applied the patch found here (https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX6DQ-ISL79985-79987-MIPI-CSI2-CVBS-cam...) , to allow display 4 camera.
It works well and i'm able to launch mxc_v4l2_tvin (up to 4 times to display 4 camera channel).
Anyway, sometimes after a while, one channel video scroll until it get resynchonized.
When it happens, i have the message
IPU WARNING IPU_INT_STAT_5=0x00000001
I've check that the isl has no error (by checking status register for each channel).
Would you have an idea of what i could check to find the problem?
Thanks in advance
Best regards
Laurent