Hello all!
I want to create correct device tree for Tianma nl10276bc13-01c with BSP for imx6qp (TQMa6x platform) .
I've built OS image and currently try to use imx6qdl-mba6-lvds-tm070jvhg33.dtsi (in attach) from kernel-4.14, which is compatible with other Tianma display:
/*
* Copyright 2018 Markus Niebel, TQ Systems GmbH
*
* The code contained herein is licensed under the GNU General Public
* License. You may obtain a copy of the GNU General Public License
* Version 2 or later at the following locations:
*
* http://www.opensource.org/licenses/gpl-license.html
* http://www.gnu.org/copyleft/gpl.html
*// {
backlight_ldb: backlight@0 {
compatible = "pwm-backlight";
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_backlight>;
pwms = <&pwm1 0 62500>;
brightness-levels = <0 16 32 64 96 128 160 192 224 255>;
default-brightness-level = <5>;
power-supply = <®_mba6_3p3v>;
enable-gpios = <&gpio4 5 GPIO_ACTIVE_HIGH>;
status = "okay";
};panel-lvds0 {
compatible = "tianma,tm070jvhg33";
backlight = <&backlight_ldb>;
power-supply = <®_mba6_3p3v>;
status = "okay";port {
panel_in_lvds0: endpoint {
remote-endpoint = <&lvds0_out>;
};
};
};
};&ldb {
status = "okay";lvds-channel@0 {
fsl,data-mapping = "spwg";
fsl,data-width = <24>;
status = "okay";port@4 {
reg = <4>;lvds0_out: endpoint {
remote-endpoint = <&panel_in_lvds0>;
};
};
};lvds-channel@1 {
status = "disabled";
};
};&iomuxc {
imx6qdl-mba6 {
pinctrl_backlight: backlightgrp {
fsl,pins = <
/* LCD.BLT_EN */
MX6QDL_PAD_GPIO_19__GPIO4_IO05 0x0001b099
>;
};
};
};
But my display has different characteristics (other size, other resolution...), so I see some poor quality when run some qt-examples (see examples below).
I cannot get what's the problem, is it related to wrong resolution or wrong color depth? And what should I change in device tree for correct display working?
解決済! 解決策の投稿を見る。
I've found wrong option in configuration after consulting with a electronics specialist, it was 'data-mapping', the right option for color map had to be 'jeida'.
Anyway, thanks.
I've found wrong option in configuration after consulting with a electronics specialist, it was 'data-mapping', the right option for color map had to be 'jeida'.
Anyway, thanks.
Hi Maksim
for custom lcd timings one can look at documentation:
https://community.nxp.com/thread/355690
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you for such useful links, I will try to get into it and try to build my device tree.
So, bad image quality is related to wrong timings, right?