Coresight On-Chip Debugging i.MX 93 - Base Addresses

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coresight On-Chip Debugging i.MX 93 - Base Addresses

1,074件の閲覧回数
silicolino
Contributor I

Hi,

for a project I want to use on-chip debugging on my imx93 (EVK). For setting up the Coresight Access Library and accessing the tracing capabilities I need the addresses for the components like ETM, ETR, ETF,... Unfortunately I cannot find them in the official documentation. Also, I am not sure if I have to set the system in a debugging state before or how I would do that. As a sidenote: I want to do the tracing in the secure world of trustzone, do I need to do any additional configuration for that?

I would be very happy about any help

Best regards

0 件の賞賛
返信
0 返答(返信)