Convert MMPF0100 PMIC - SW3A/B to single phase output.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Convert MMPF0100 PMIC - SW3A/B to single phase output.

724 次查看
mrudangshelat
Contributor IV
Hi,
In my iMX6D based design, we have used the MMPF0100 to supply voltage and CPU/SOC core voltages and it's interface devices.
I have received my board and started testing. I have made a design with SW3A/B Dual Phase output, and I am getting SW3A (VDD_1V5_3A - DDR3L Interface) - 1.5V  and SW3B (VDD_1V5_3B - floating output) - 2.1 floating voltage.
To keep both SW3A/B with high current output, I would like to convert it PMIC SW3A/B Dual Phase to SW3A/B single Phase output. Kindly provide me changes required to make in my existing design SW3A/B with 1.5V with a 2.5Amp output.

Please find attached PMIC schematic. 

 
Awaiting for your earlier response.
标签 (1)
0 项奖励
回复
1 回复

579 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 Section 6.4.4.4.5 (SW3A/B single phase) of the PF0100 Datasheet describes

single phase mode, and Figure 21 (SW3A/B single phase block diagram)

clarifies schematic implementation for it.

 

  Note :

According to Table 10 (Start-up configuration) of the PF0100 Datasheet,

SW3AB Single Phase, 2.0 MHz is start up setting for SW3.

 

http://www.nxp.com/assets/documents/data/en/data-sheets/MMPF0100.pdf 

 

Summary page :

Configurable PMICs (PF Series)|NXP 

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复