Connector used for iMX7 Dual evaluation board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connector used for iMX7 Dual evaluation board

595件の閲覧回数
toshiharu_shimi
Contributor I

hello,Community

I would like to connect i.MX7Dual evaluation board "iMX7DSABRE"  to LCD that have MIPI interface.

What is the connector maker and product number used for MIPI DSI Connector (DSI_CONN (J30))?

Documents of  iMX7DSABRE "SCH-28590_I.MX7D_SABER_REV_D_160314.xls" describe bellow.

"BTB Connector,socket,Right Angle,24Pin,0.4MM Pitch,1.5MM Height,Au,Black,SMD"

But, I am not sure what connector is used here.

Best Regards,

Toshiharu Shimizu

ラベル(1)
0 件の賞賛
返信
1 返信

508件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Toshiharu

one can check

SABER i.MX 7Dual J30 connector 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信