Connect OV5640 Camera Module to Sabre Board.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Connect OV5640 Camera Module to Sabre Board.

3,801 Views
admin
Specialist II

Hi all,

I want to connect an OV5640 Camera Module to the Sabre Board. The current camera module in Sabre is OV4642. It is similar to OV5640. there are both ov5640.c and ov5642.c in the kernel_imx/drivers/media/video/mxc/capture folder.

Can anyone tell me how to config the Sabre board and make OV5640 work, instead of OV5640.

Thanks all.

7 Replies

1,348 Views
lily_zhang
NXP Employee
NXP Employee

Are you using MX6 SabreSD board? By using default image, you jus need to put OV5640 camera sensor into MIPI port.

Besides configuration, you should check arch/arm/mach-mx6/board-mx6q_sabresd.c.

For example:

        {

                I2C_BOARD_INFO("ov5642", 0x3c),

                .platform_data = (void *)&camera_data,

        },

        {

                I2C_BOARD_INFO("ov5640_mipi", 0x3c),

                .platform_data = (void *)&mipi_csi2_data,

        },

....

0 Kudos
Reply

1,348 Views
GaoJianzhong
Contributor IV

Yes,it is SabreSD board.

The problem is that i don't know where can i buy the OV5640 camera module.

0 Kudos
Reply

1,348 Views
hyunhoshin
Contributor III


me too!

0 Kudos
Reply

1,348 Views
lily_zhang
NXP Employee
NXP Employee

One information is FYI:

The cameras on the boards come from Omnivision (Ordering Number: OV05640-MRFL-AA0T) and can be ordered through distributor Nu Horizons for example (see http://www.nuhorizons.com/).

0 Kudos
Reply

1,348 Views
lily_zhang
NXP Employee
NXP Employee

Please contact your support window and see whether he can help you to find camera sensors.

0 Kudos
Reply

1,348 Views
GaoJianzhong
Contributor IV

Hi

I want to buy the ov5640 module for sabre sd board,

Where did you get it?

Thank you.

0 Kudos
Reply

1,348 Views
janiscoders
Contributor III

Did you succeed in configuring kernel for ov5640 ?

We are trying to do the same thing without success.

Can someone please help me with this by providing some hints?

Thank you

0 Kudos
Reply