Configuring the resolution of the VGA to support 800x600 and 640x480

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring the resolution of the VGA to support 800x600 and 640x480

1,446 Views
ShishirJha
Contributor I

Hello to all,

I have been working with imx53 board for last few days and am loving it. I have android up and running, but ran into resolution problem. The screen that I want to use the imx53 for is 800x600 or even better if it is 800x480. Present resolution of 1024x768 was good on a monitor but the touch panel that I have now will not accept that resolution. Though I have the task of integrating the touch screen driver in the kernel still ahead of me, I would like to get the resolution right first. I am using the VGA port and not the LVDS output for the touch panel display. 

Looking at the Kernel Source it looks like I need to edit the frame buffer definitions in mx53loco.c but I am not sure what values to input there to define a mode for 800x600 and 800x480. 

Any help in this matter would be great. 

Also, has anyone tried soldering a momentary push button switch on to the Power button to get the Power button out on a case for switching the board on and off. I am skeptical on whether I should do it or not and if it would affect the PMIC in any way. 

Regards

Labels (1)
0 Kudos
Reply
3 Replies

1,070 Views
ShishirJha
Contributor I

Thank you Phil and Luis for your help, it guided me to the right path and all that I needed to was change the vga line from VGA-XGA to VGA-SVGA in the uboot to get force it to 800x600. This was defined in tve.c.

0 Kudos
Reply

1,070 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

 

800x600x16bpp and 800x600x32bpp are supported in the BSP, see BSP release notes for kernel parameters.

 

These app notes can help you:

 

http://www.freescale.com/webapp/search/Serp.jsp?qt=different+display&QueryText=different+display&bas...



You can check the following application notes:

AN3974 : Different Display Configurations on i.MX35 Linux PDK
AN4182 : Different Display Configurations on the i.MX31 Linux PDK

 

See also, chapter 18:

 

http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf?fpsp=1&WT_TYPE=Users%20Guides&WT_VE...

 

Have a look to static struct fb_videomode video_modes_vga[] in tve.c

You will have to add new entry in the struct and a new 'CASE' in 'int tve_setup(int mode)'

Best Regards,

0 Kudos
Reply

1,070 Views
PhilEndecott
Contributor II
Yes, you need to hack the kernel. No, I don't know the values that you need. Yes, I believe that you should be able to extend the power-on button in the way that you propose without any trouble.
0 Kudos
Reply