Configuring Display Interface For a new LCD(i.MX53).

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring Display Interface For a new LCD(i.MX53).

Jump to solution
1,441 Views
ricardo_ioct
Contributor III

Hello, Community.

Recently, I'm trying to interface a Trully LCD. It's a 240x320(portrait) display, with RGB666 interface, VSYNC, HSYNC, PIXCLK and DE signals. Looking for references on Linux kernel(on arch files of the QSB board and SABRE), and reading IMX53 User Manual, I figured out that some pins of the DI module(DI0_PINxx) can act as VSYNC, HSYNC and DE, but I don't realize where in the BSP each generic pin is assigned with a specific function. Can someone help me?

For the record: on mx53_loco.c file, those pads are configured as sync pins:

MX53_PAD_DI0_PIN15__IPU_DI0_PIN15,
MX53_PAD_DI0_PIN2__IPU_DI0_PIN2,
MX53_PAD_DI0_PIN3__IPU_DI0_PIN3,

On QSB schematic, they are, respectively, DE, HSYNC and VSYNC. As these IPU pins are generics, I want to know where they are specifically configured.

Regards,

Ricardo Gurgel.

Labels (2)
0 Kudos
1 Solution
644 Views
jimmychan
NXP TechSupport
NXP TechSupport

1. http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Please read the Chapter 18 for LCD porting details.

2.  Different Display Configurations on i.MX35 Linux PDK

http://cache.freescale.com/files/dsp/doc/app_note/AN3974.pdf

Although this is for i.MX35, the driving porting in Linux for i.MX53 is the same.

View solution in original post

0 Kudos
1 Reply
645 Views
jimmychan
NXP TechSupport
NXP TechSupport

1. http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Please read the Chapter 18 for LCD porting details.

2.  Different Display Configurations on i.MX35 Linux PDK

http://cache.freescale.com/files/dsp/doc/app_note/AN3974.pdf

Although this is for i.MX35, the driving porting in Linux for i.MX53 is the same.

0 Kudos