Does there is some source code available for the gal2d api? There is some test application in the linux packages, but it look like the source code of the application is not available... There is a package named gpu-viv-src listed in ltib, but I cannot download it:
./ltib -m prep --pkg gpu-viv-src
Processing: gpu-viv-src
=========================
Build path taken because: build key set, no prebuilt rpm,
Testing network connectivity
OK GPP:
Try gpu-viv-src-1.1.0.tar.gz.md5 from the GPP
http://bitshrine.org/gpp/gpu-viv-src-1.1.0.tar.gz.md5:
16:53:38 ERROR 404: Not Found.
Try gpu-viv-src-1.1.0.tar.gz from the GPP
http://bitshrine.org/gpp/gpu-viv-src-1.1.0.tar.gz:
16:53:39 ERROR 404: Not Found.
Can't get: gpu-viv-src-1.1.0.tar.gz at ./ltib line 802.
Does the source code of the test application that is using the GC320 in fb mode is available?