Component Usuage for iMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Component Usuage for iMX6

1,020件の閲覧回数
sarasur
Contributor II

I am using PEx for first time. I have imported components library from McuOnEclipse download | SourceForge.net Can I use these components for iMX6DL development?

0 件の賞賛
返信
3 返答(返信)

733件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

The components that you are mentioning are to be used with ARM microcontrollers (Kinetis), while i.MX6 is an Applications Processor, so they are not compatible. You could take a look at the following link:

Overview: Processor Expert | MCU on Eclipse

For i.MX6, you have other options like the Linux and Android BSPs.


Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

733件の閲覧回数
sarasur
Contributor II

Thank you Carlos for your prompt suggestion.

However I am trying to do bare metal program for LED blink (so Linux and Android BSPs does not solve the purpose). The link Overview: Processor Expert | MCU on Eclipse  gives the details about using the components for Kinetis (as you rightly said, however not iMX6).

I have installed PEx v1.1 which shows components library with PinSettings Component only. Check the attached .jpeg

How do I start with bare metal for LED blink?

Best Regards,

Sarang

PEx_plugins.jpg

0 件の賞賛
返信

733件の閲覧回数
alubeiro
Contributor IV

Hi Sarang,

I am in the same situation.

Finally, did you achieve to get or import more components?

I find so wierd that even in the CPU component, one can't configurate any parameter.

Thanks and best regards

0 件の賞賛
返信