Clock source of i.MX6 HDMI TMDS and audio clock.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Clock source of i.MX6 HDMI TMDS and audio clock.

ソリューションへジャンプ
1,351件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a simple question about the clock source of i.MX6 HDMI TMDS and audio clock.

I guess the clock source of TMDS is video_27m_clk_root from PLL3 PFD1 and HDMI audio clock is regenerated from TMDS with N and CTS.

Is this correct?

Best Regards,

Satoshi Shimoda

ラベル(5)
タグ(1)
0 件の賞賛
返信
1 解決策
1,012件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think yes, this is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,013件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I think yes, this is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,012件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Igor,

Thank you for your reply.

Then, would you let me know the tolerance of HDMI audio clock which is made by TMDS clock also?

(e.g. +- xx%)

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信
1,012件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

please check

IMX6DQ6SDLHDG  Table 2-20. 24 MHz crystal tolerance guidelines

Best regards

igor