Chromium on IMX8QM hardware acceleration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Chromium on IMX8QM hardware acceleration

1,722件の閲覧回数
guojing_7
Contributor I

Hi,  I want to use Chromium's hardware acceleration on IMX8QM through V4L2, but it not work!

The following link describe the issue, does anybody met this problem? 

https://github.com/OSSystems/meta-browser/issues/281

0 件の賞賛
返信
2 返答(返信)

1,466件の閲覧回数
theguybieber
Contributor I

Are there yocto recipes available for Chromium on imx8 quadmax? What is the most performant browser to use here?

 

0 件の賞賛
返信

1,549件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi guo

unfortunately it is not supported in nxp linux, sorry.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信