Hello,
I'm using Yocto Langdale release for IMX8MM. According to this commit message, V4L2 hardware video decoding should be enabled in Chromium with this release:
commit fe0d3587d905a8fa32a9830d177f97c90352fdc5
- support on i.MX 8 series platform. - 8MM/8MP/8MQ support h264/hevc/vp8/vp9 hardware decoding. - 8QM/8QXP support h264/hevc/vp8 hardware decoding. - support seek, playrate change and resolution change. - support video acceleration for online media platform such as Youtube, bilibili. Signed-off-by: Hou Qi <qi.hou@nxp.com>
解決済! 解決策の投稿を見る。
Hello @PiotrKrygier ,
I hope you are doing well.
Please refer to the below-given link for reference.
https://community.nxp.com/t5/
Thanks & Regards,
Sanket Parekh
Hello @PiotrKrygier ,
I hope you are doing well.
I'm happy to help you.
"I managed to fix the problem. It was fortunately not related to code itself but to the faulty sd card, that was used to hold the image."
As the Issue is solved now, hence Can I close the case?
Thanks & Regards,
Sanket Parekh
Yes, thank you. The issue can be closed now.