Change the voltage level of eim pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Change the voltage level of eim pin

677件の閲覧回数
wenyubo
Contributor I

hi:

Do someone knows the voltage level of the imx6q eim pin can change to 1.8v(default is 3.3v).

thank you very much! 

ラベル(4)
0 件の賞賛
3 返答(返信)

560件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wen

NVCC_EIMx should be changed, please check Table 6. Operating Ranges,

Table 100. 21 x 21 mm Functional Contact Assignments i.MX6DQ Datasheet

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛

560件の閲覧回数
wenyubo
Contributor I

but what registers to configure,can you explain,thank you!  

0 件の賞賛

560件の閲覧回数
michel_renker
Contributor I

Hello, i've got the same problem and i would like to ask, if you found a solution. Does the configuration works with registers and when yes, which one you have to set?

Thanks.

0 件の賞賛