Cascading Interrupts through I2C Muxer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cascading Interrupts through I2C Muxer

656 Views
malik_cisse
Senior Contributor I

We use 3 adps9960 chips in our design (see schematic bellow) that are connected to an i2c muxer (PCA9544A).

I am struggling passing the APDS9960 interrupts to the CPU.

Could someone share a device tree example for this. Bellow is the device tree I am using right now.

The Interrupts are correctly seen in PCA9544A i2c Muxer driver but they are not forwarded to APDS-9960 driver.

malik_cisse_0-1674820962020.png

Current Device Tree:

&i2c4 {

    pinctrl-names = "default","gpio";

    pinctrl-0 = <&pinctrl_i2c4>;

    pinctrl-1 = <&pinctrl_i2c4_gpio>;

    sda-gpios = <&gpio5 21 (GPIO_ACTIVE_HIGH | GPIO_OPEN_DRAIN)>;

    scl-gpios = <&gpio5 20 (GPIO_ACTIVE_HIGH | GPIO_OPEN_DRAIN)>;

    clock-frequency = <400000>;

    status = "okay";

 

    i2c4_mux_apds: i2c4-mux-pca9544@70 {

        compatible = "nxp,pca9544";

        #address-cells = <1>;

        #size-cells = <0>;

        reg = <0x70>;      

        pinctrl-names = "default";

        pinctrl-0 = <&pinctrl_pca9544a_70>;

        interrupt-parent = <&gpio2>;

        interrupts = <6 IRQ_TYPE_EDGE_FALLING>;

        interrupt-controller;

        #interrupt-cells = <2>;

 

        i2c@0 {

            #address-cells = <1>;

            #size-cells = <0>;

            reg = <0>;

 

            proximity@39 {

                compatible = "avago,apds9960";

                reg = <0x39>; 

                interrupt-parent = <&i2c4_mux_apds>; //unsure about this ???

                interrupts = <0 2>;//unsure about this ???

                };

        };

 

        i2c@1 {

            #address-cells = <1>;

            #size-cells = <0>;

            reg = <1>;

 

            proximity@39 {

                compatible = "avago,apds9960";

                reg = <0x39>;

                interrupt-parent = <&i2c4_mux_apds>;

                interrupts = <1 2>;

                };

        };

 

        i2c@2 {

            #address-cells = <1>;

            #size-cells = <0>;

            reg = <2>;

 

            proximity@39 {

                compatible = "avago,apds9960";

                reg = <0x39>;

                interrupt-parent = <&i2c4_mux_apds>;

                interrupts = <2 2>;

                };

        };

 

        i2c@3 {

            #address-cells = <1>;

            #size-cells = <0>;

            reg = <3>;

            /* NC */

        };

 

    };

 

…..

 

&iomuxc {

    pinctrl_pca9544a_70: pinctrl-pca9544-70 {

        fsl,pins = <

            MX8MP_IOMUXC_SD1_DATA4__GPIO2_IO06      0x52

        >;

    };

 

Thank you

 

Labels (1)
0 Kudos
Reply
2 Replies

624 Views
malik_cisse
Senior Contributor I

Thank you Aldo,
I have tried this implementation but for some strange reasons, the interrupt does not get dispatched to the lower level driver.

0 Kudos
Reply

633 Views
AldoG
NXP TechSupport
NXP TechSupport
0 Kudos
Reply