After the long run, some customer systems are fail with the following error:
mmc2: Card stuck in programming state! mmcblk2 card_busy_detect
mmc2: cache flush error -110
mmc2: tried to reset card, got error -110
print_req_error: I/O error, dev mmcblk2, sector 6005384
EXT4-fs warning (device mmcblk2p2): ext4_end_bio:323: I/O error 10 writing to inode 38386 (offset 0 size 0 starting block 750674)
Buffer I/O error on device mmcblk2p2, logical block 725073
EXT4-fs warning (device mmcblk2p2): ext4_end_bio:323: I/O error 10 writing to inode 38386 (offset 4530176 size 4096 starting block 750675)
Buffer I/O error on device mmcblk2p2, logical block 725074
JBD2: Detected IO errors while flushing file data on mmcblk2p2-8
The full customer log include the SDHCI Register dump attached.
Kernel 4.14.98
Any suggestion will be highly appreciated
Hi
Can customer test the latest kernel?
Best Regards
Zhiming