Cant BOOT IMX6 QUAD with Plugin Mode enabled SPL and u-boot.bin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cant BOOT IMX6 QUAD with Plugin Mode enabled SPL and u-boot.bin

840件の閲覧回数
manojsampathkum
Contributor II

Hi

I have enabled the plugin Mode in u-boot and I am trying to boot QUAD with  SPL and u-boot.bin combination. I am doing for a test case. I flashed those images using MFGTOOLS. When i tried to boot , it is not booting am not getting any log in minicom. But it boots perfectly when i use u-boot.imx instead of SPL and u-boot.bin.

After that i found the fix for  not booting with SPL and u-boot.bin . 

To solve issue in booting SPL  with plugin mode, I am booting it in DDR memory instead of internal SRAM memory.

what is the reason  behind i am not able to boot it in the internal SRAM ??

Is there any restriction  with the plugin mode booting??

Regards

Manoj

ラベル(2)
0 件の賞賛
1 返信

663件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Manoj

reason may be that uboot size is too big for internal SRAM memory,

also this may be posted on uboot mail list:

U-Boot Info Page 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛