Hello,
I am trying to enter into recovery mode in iMX6ULL processor (using Colibri Evaluation Board). I am following the official documentation of the steps but still not able to enter into the recovery mode.
When I view the list of USB devices after (I assume) entering the recovering mode, the device is not recognized. The list shows:
Error USB Unknown USB Device (Device Descriptor Request Failed) USB\VID_...
I tried ignoring this error and tried to load the recovery-windows.bat file which outputs two different errors as follows:
1. When I first run the .bat file:
config file <recovery\\\imx_usb.conf>
vid=0x15a2 pid=0x0054 file_name=mx6_usb_rom.conf
-> vid=0x1b67 pid=0x4fff file_name=mx6_usb_sdp_spl.conf
-> vid=0x1b67 pid=0x4000 file_name=mx6_usb_sdp_uboot.conf
vid=0x15a2 pid=0x0061 file_name=mx6_usb_rom.conf
-> vid=0x1b67 pid=0x4fff file_name=mx6_usb_sdp_spl.conf
-> vid=0x1b67 pid=0x4000 file_name=mx6_usb_sdp_uboot.conf
vid=0x15a2 pid=0x0076 file_name=mx7_usb_rom.conf
-> vid=0x1b67 pid=0x4000 file_name=mx7_usb_sdp_uboot.conf
vid=0x15a2 pid=0x0080 file_name=mx6ull_usb_rom.conf
-> vid=0x1b67 pid=0x4000 file_name=mx6ull_usb_sdp_uboot.conf
config file <recovery\\\mx6ull_usb_rom.conf>
parse recovery\\\mx6ull_usb_rom.conf
Trying to open device vid=0x15a2 pid=0x0080
Interface 0 claimed
HAB security state: development mode (0x56787856)
== work item
filename u-boot-nand.imx
load_size 0 bytes
load_addr 0x83f00000
dcd 1
clear_dcd 0
plug 0
jump_mode 2
jump_addr 0x00000000
== end work item
loading DCD table @0x910000
<<<-536, 1024 bytes>>>
succeeded (status 0x128a8a12)
loading binary file(u-boot-nand.imx) to 877ff000, skip=0, fsize=88000 type=aa
<<<557056, 557056 bytes>>>
succeeded (status 0x88888888)
jumping to 0x877ff400
config file <recovery\\\mx6ull_usb_sdp_uboot.conf>
parse recovery\\\mx6ull_usb_sdp_uboot.conf
Trying to open device vid=0x1b67 pid=0x4000.........................
Could not open device vid=0x1b67 pid=0x4000
Press any key to continue . . .
2. When I run the .bat file again and again:
config file <recovery\\\imx_usb.conf>
vid=0x15a2 pid=0x0054 file_name=mx6_usb_rom.conf
-> vid=0x1b67 pid=0x4fff file_name=mx6_usb_sdp_spl.conf
-> vid=0x1b67 pid=0x4000 file_name=mx6_usb_sdp_uboot.conf
vid=0x15a2 pid=0x0061 file_name=mx6_usb_rom.conf
-> vid=0x1b67 pid=0x4fff file_name=mx6_usb_sdp_spl.conf
-> vid=0x1b67 pid=0x4000 file_name=mx6_usb_sdp_uboot.conf
vid=0x15a2 pid=0x0076 file_name=mx7_usb_rom.conf
-> vid=0x1b67 pid=0x4000 file_name=mx7_usb_sdp_uboot.conf
vid=0x15a2 pid=0x0080 file_name=mx6ull_usb_rom.conf
-> vid=0x1b67 pid=0x4000 file_name=mx6ull_usb_sdp_uboot.conf
config file <recovery\\\mx6ull_usb_rom.conf>
parse recovery\\\mx6ull_usb_rom.conf
Trying to open device vid=0x15a2 pid=0x0080
Any help would be highly appreciated. Thank you !!
Hi @user_Gaurav,