Cannot flash the I.MX6 SoloX-based board on Linux. Error: [Failure to claim interface]

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Cannot flash the I.MX6 SoloX-based board on Linux. Error: [Failure to claim interface]

跳至解决方案
1,250 次查看
andriibr
Contributor II

Hello,

I have an issue with flashing the iMX6 SoloX COM board from Embedded Artists
using uuu.

Info about the board:

https://www.embeddedartists.com/products/imx6-solox-com

I'm following the flash guide below:

https://developer.embeddedartists.com/docs-app/yocto/deploy-images

 

The steps I take based on the flashing guide:

1) Power ON, switch the board into OTG mode, and reset.

2) Launch the uuu app with a flash script as an argument.

./uuu full_tar.uuu

Flash script contents:

uuu_version 1.0.1

SDP: boot -f firmware/u-boot.imx

FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: ucmd mmc dev ${emmc_dev}

FB: ucmd setenv fastboot_buffer ${loadaddr}
FB: download -f firmware/zImage
FB: ucmd setenv fastboot_buffer ${fdt_addr}
FB: download -f firmware/kit_v2.dtb
FB: ucmd setenv fastboot_buffer ${initrd_addr}
FB: download -f firmware/fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot
FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}

# Wait for emmc
FBK: ucmd while [ ! -e /dev/mmcblk*boot0 ]; do sleep 1; echo "wait for /dev/mmcblk*boot* appear"; done;

# get emmc device
FBK: ucmd dev=`ls /dev/mmcblk*boot*`; dev=($dev); dev=${dev[0]}; dev=${dev#/dev/mmcblk}; dev=${dev%boot*}; echo $dev > /tmp/mmcdev;

# create partition
FBK: ucmd mmc=`cat /tmp/mmcdev`; PARTSTR=$'4M,10M,0c\n14M,,83\n'; echo "$PARTSTR" | sfdisk --force /dev/mmcblk${mmc}

# format partition
FBK: ucmd mmc=`cat /tmp/mmcdev`; mkfs.vfat /dev/mmcblk${mmc}p1
FBK: ucmd mkdir -p /mnt/fat
FBK: ucmd mmc=`cat /tmp/mmcdev`; mount -t vfat /dev/mmcblk${mmc}p1 /mnt/fat

# erase u-boot environment (8Kb located at offset (2Mb-8Kb) on /dev/mmcblk*boot0)
FBK: ucmd mmc=`cat /tmp/mmcdev`; echo 0 > /sys/block/mmcblk${mmc}boot0/force_ro
FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/dev/zero of=/dev/mmcblk${mmc}boot0 bs=1k seek=2040 count=8

# bootloaders (SPL + u-boot)
FBK: ucp files/SPL t:/tmp
FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/tmp/SPL of=/dev/mmcblk${mmc}boot0 bs=512 seek=2
FBK: ucp files/u-boot.img t:/tmp
FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/tmp/u-boot.img of=/dev/mmcblk${mmc}boot0 bs=512 seek=138
FBK: ucmd mmc=`cat /tmp/mmcdev`; echo 1 > /sys/block/mmcblk${mmc}boot0/force_ro
FBK: ucmd mmc=`cat /tmp/mmcdev`; mmc bootpart enable 1 1 /dev/mmcblk${mmc}

# Copy kernel and dtb files
FBK: ucp files/zImage t:/mnt/fat/zImage
FBK: ucp files/kit_v2.dtb t:/mnt/fat
FBK: ucp files/kit_v2-m4.dtb t:/mnt/fat
FBK: ucp files/boot.scr t:/mnt/fat
FBK: ucp files/m4_hello_ddr.bin t:/mnt/fat
FBK: ucp files/m4_hello_ocram.bin t:/mnt/fat
FBK: ucp files/m4_hello_qspi.bin t:/mnt/fat
FBK: ucp files/m4_hello_tcm.bin t:/mnt/fat
FBK: ucp files/m4_rpmsg_ping_qspi.bin t:/mnt/fat
FBK: ucmd umount /mnt/fat
FBK: ucmd mmc=`cat /tmp/mmcdev`; mkfs.ext3 -F -E nodiscard -j /dev/mmcblk${mmc}p2
FBK: ucmd mkdir -p /mnt/ext3
FBK: ucmd mmc=`cat /tmp/mmcdev`; mount -t ext3 /dev/mmcblk${mmc}p2 /mnt/ext3
FBK: acmd export EXTRACT_UNSAFE_SYMLINKS=1; tar -jx -C /mnt/ext3
FBK: ucp files/orion-image-base.tar.bz2 t:-
FBK: Sync
FBK: ucmd umount /mnt/ext3

FBK: DONE

 

The output I get:

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-0-gaeb3490

Success 0 Failure 0


1:10 1/ 1 [=================100%=================] SDP: boot -f firmware/u-boot.imx

 

Then, uuu just hangs. But because the bootloader is already in RAM I do the
following:

 

3) Open minicom -D /dev/ttyUSB0.

The output of u-boot to the serial console via UART:

Welcome to minicom 2.8

OPTIONS: I18n
Port /dev/ttyUSB0, 15:16:12

Press CTRL-A Z for help on special keys

�4�W'$HNMevices, 19 uclasses, devicetree: separate
PMIC: PFUZE100! DEV_ID=0x11 REV_ID=0x21
MMC: FSL_SDHC: 2, FSL_SDHC: 3
Loading Environment from MMC... OK
In: serial
Out: serial
Err: serial
switch to partitions #0, OK
mmc2(part 0) is current device
Saving Environment to MMC... Writing to MMC(2)... OK
flash target is MMC:2
Net: eth0: ethernet@2188000 [PRIME]Get shared mii bus on ethernet@21b4000
FEC0:1 is connected to ethernet@2188000. Reconnecting to ethernet@21b4000
, eth1: ethernet@21b4000
Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for mfgtools
, using default environment

Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else bootz ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run;
Hit any key to stop autoboot: 0
=>

 

For whatever reason, `bootcmd_mfg` didn't execute anything, so I manually ran the
bootcmd.

run bootcmd_mfg

 

This puts the board into fastboot mode, and the flashing process resumes.

=> run bootcmd_mfg

## Checking Image at 83800000 ...
Unknown image format!
Run fastboot ...
switch to partitions #0, OK
mmc2(part 0) is current device
Starting download of 9275008 bytes
......................................................................
downloading of 9275008 bytes finished
Starting download of 50797 bytes

downloading of 50797 bytes finished
Starting download of 12514332 bytes
..........................................................................
.....................
downloading of 12514332 bytes finished
Kernel image @ 0x80800000 [ 0x000000 - 0x8d8680 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
Image Name: fsl-image-mfgtool-initramfs-imx6
Image Type: ARM Linux RAMDisk Image (uncompressed)
Data Size: 12514268 Bytes = 11.9 MiB
Load Address: 00000000
Entry Point: 00000000
Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Using Device Tree in place at 83000000, end 8300f66c
No PMIC found!

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 5.15.32+geb06aa0de7de (oe-user@oe-host) (arm-poky-linux-gnueabi-gcc (GCC) 11.2.0, GNU ld (GNU Binutils) 2.38.20220313) #1 SMP PREEMPT Tue Mar 21 15:39:28 UTC 2023
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: Embedded Artists i.MX6 SoloX COM Kit
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] Reserved memory: created CMA memory pool at 0xac000000, size 320 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Zone ranges:
[ 0.000000] Normal [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] HighMem empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
[ 0.000000] percpu: Embedded 12 pages/cpu s17036 r8192 d23924 u49152
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 259840
[ 0.000000] Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc clk_ignore_unused
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 677528K/1048576K available (12288K kernel code, 1374K rwdata, 4256K rodata, 1024K init, 422K bss, 43368K reserved, 327680K cma-reserved, 0K highmem)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] L2C-310 erratum 769419 enabled
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[ 0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 256 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76430001
[ 0.000000] random: get_random_bytes called from start_kernel+0x484/0x64c with crng_init=0
[ 0.000000] Switching to timer-based delay loop, resolution 333ns
[ 0.000001] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[ 0.000029] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[ 0.001657] Console: colour dummy device 80x30
[ 0.001705] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.001725] pid_max: default: 32768 minimum: 301
[ 0.001877] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.001901] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes, linear)
[ 0.002706] CPU: Testing write buffer coherency: ok
[ 0.002757] CPU0: Spectre v2: using BPIALL workaround
[ 0.002964] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.003641] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.003822] rcu: Hierarchical SRCU implementation.
[ 0.004140] smp: Bringing up secondary CPUs ...
[ 0.004156] smp: Brought up 1 node, 1 CPU
[ 0.004170] SMP: Total of 1 processors activated (6.00 BogoMIPS).
[ 0.004183] CPU: All CPU(s) started in SVC mode.
[ 0.004619] devtmpfs: initialized
[ 0.012746] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.012970] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.012999] futex hash table entries: 256 (order: 2, 16384 bytes, linear)
[ 0.031924] pinctrl core: initialized pinctrl subsystem
[ 0.033028] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.039912] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.041153] thermal_sys: Registered thermal governor 'step_wise'
[ 0.041411] cpuidle: using governor menu
[ 0.057374] vdd1p1: supplied by regulator-dummy
[ 0.058019] vdd3p0: supplied by regulator-dummy
[ 0.058603] vdd2p5: supplied by regulator-dummy
[ 0.059490] vddpcie: supplied by regulator-dummy
[ 0.060442] mxs_phy 20c9000.usbphy: supply phy-3p0 not found, using dummy regulator
[ 0.061151] mxs_phy 20ca000.usbphy: supply phy-3p0 not found, using dummy regulator
[ 0.080560] No ATAGs?
[ 0.080626] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.080645] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.082805] imx6sx-pinctrl 20e0000.pinctrl: initialized IMX pinctrl driver
[ 0.085376] imx mu driver is registered.
[ 0.086049] imx rpmsg driver is registered.
[ 0.087424] MU is ready for cross core communication!
[ 0.117646] lcd-3v3 GPIO handle specifies active low - ignored
[ 0.121198] vgaarb: loaded
[ 0.122036] SCSI subsystem initialized
[ 0.122503] usbcore: registered new interface driver usbfs
[ 0.122566] usbcore: registered new interface driver hub
[ 0.122616] usbcore: registered new device driver usb
[ 0.122780] usb_phy_generic usbphynop1: supply vcc not found, using dummy regulator
[ 0.125187] i2c i2c-0: IMX I2C adapter registered
[ 0.126180] pca953x 1-0020: using no AI
[ 0.130854] pca953x 1-0020: failed writing register
[ 0.130953] i2c i2c-1: IMX I2C adapter registered
[ 0.131541] i2c i2c-2: IMX I2C adapter registered
[ 0.132036] mc: Linux media interface: v0.10
[ 0.132101] videodev: Linux video capture interface: v2.00
[ 0.132215] pps_core: LinuxPPS API ver. 1 registered
[ 0.132228] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.132252] PTP clock support registered
[ 0.134474] MIPI CSI2 driver module loaded
[ 0.134535] Advanced Linux Sound Architecture Driver Initialized.
[ 0.135701] Bluetooth: Core ver 2.22
[ 0.135768] NET: Registered PF_BLUETOOTH protocol family
[ 0.135781] Bluetooth: HCI device and connection manager initialized
[ 0.135801] Bluetooth: HCI socket layer initialized
[ 0.135815] Bluetooth: L2CAP socket layer initialized
[ 0.135840] Bluetooth: SCO socket layer initialized
[ 0.136416] clocksource: Switched to clocksource mxc_timer1
[ 0.136632] VFS: Disk quotas dquot_6.6.0
[ 0.136714] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.145134] NET: Registered PF_INET protocol family
[ 0.145332] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.146537] tcp_listen_portaddr_hash hash table entries: 512 (order: 0, 6144 bytes, linear)
[ 0.146587] TCP established hash table entries: 8192 (order: 3, 32768 bytes, linear)
[ 0.146671] TCP bind hash table entries: 8192 (order: 4, 65536 bytes, linear)
[ 0.146801] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.146926] UDP hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.146978] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes, linear)
[ 0.147173] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.147818] RPC: Registered named UNIX socket transport module.
[ 0.147840] RPC: Registered udp transport module.
[ 0.147849] RPC: Registered tcp transport module.
[ 0.147858] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.147874] PCI: CLS 0 bytes, default 64
[ 0.148384] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[ 0.150793] Bus freq driver module loaded
[ 0.151680] Initialise system trusted keyrings
[ 0.151909] workingset: timestamp_bits=14 max_order=18 bucket_order=4
[ 0.156738] Trying to unpack rootfs image as initramfs...
[ 0.167525] NFS: Registering the id_resolver key type
[ 0.167565] Key type id_resolver registered
[ 0.167578] Key type id_legacy registered
[ 0.167631] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.168138] fuse: init (API version 7.34)
[ 0.366677] Key type asymmetric registered
[ 0.366702] Asymmetric key parser 'x509' registered
[ 0.366797] io scheduler mq-deadline registered
[ 0.366814] io scheduler kyber registered
[ 0.373942] pwm-backlight backlight1: supply power not found, using dummy regulator
[ 0.377659] pwm-backlight backlight2: supply power not found, using dummy regulator
[ 0.401176] mxs-dma 1804000.dma-apbh: initialized
[ 0.419220] pfuze100-regulator 0-0008: Full layer: 2, Metal layer: 1
[ 0.419938] pfuze100-regulator 0-0008: FAB: 0, FIN: 0
[ 0.419965] pfuze100-regulator 0-0008: pfuze200 found.
[ 0.436395] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 30, base_baud = 5000000) is a IMX
[ 1.530984] random: fast init done
[ 2.089271] Freeing initrd memory: 12224K
[ 2.089437] imx-sdma 20ec000.sdma: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2
[ 2.089454] imx-sdma 20ec000.sdma: Falling back to sysfs fallback for: imx/sdma/sdma-imx6q.bin
[ 2.115364] printk: console [ttymxc0] enabled
[ 2.121066] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 78, base_baud = 5000000) is a IMX
[ 2.130604] 21f4000.serial: ttymxc4 at MMIO 0x21f4000 (irq = 79, base_baud = 5000000) is a IMX
[ 2.141580] imx sema4 driver is registered.
[ 2.164918] brd: module loaded
[ 2.174276] loop: module loaded
[ 2.177694] at24 0-0055: supply vcc not found, using dummy regulator
[ 2.185254] at24 0-0055: 8192 byte 24c64 EEPROM, writable, 32 bytes/write
[ 2.193438] imx ahci driver is registered.
[ 2.202486] spi-nor spi5.0: is25lp064 (8192 Kbytes)
[ 2.209515] spi-nor spi5.2: is25lp064 (8192 Kbytes)
[ 2.218944] CAN device driver interface
[ 2.228150] pps pps0: new PPS source ptp0
[ 2.247731] fec 2188000.ethernet eth0: registered PHC device 0
[ 2.255291] pps pps1: new PPS source ptp1
[ 2.263067] fec 21b4000.ethernet eth1: registered PHC device 1
[ 2.269546] e1000e: Intel(R) PRO/1000 Network Driver
[ 2.274524] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 2.281267] usbcore: registered new interface driver r8152
[ 2.286928] usbcore: registered new interface driver lan78xx
[ 2.292643] usbcore: registered new interface driver asix
[ 2.298133] usbcore: registered new interface driver ax88179_178a
[ 2.304266] usbcore: registered new interface driver cdc_ether
[ 2.310177] usbcore: registered new interface driver smsc95xx
[ 2.315961] usbcore: registered new interface driver net1080
[ 2.321688] usbcore: registered new interface driver cdc_subset
[ 2.327669] usbcore: registered new interface driver zaurus
[ 2.333279] usbcore: registered new interface driver MOSCHIP usb-ethernet driver
[ 2.340754] usbcore: registered new interface driver cdc_ncm
[ 2.346448] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.352982] ehci-pci: EHCI PCI platform driver
[ 2.357534] usbcore: registered new interface driver usb-storage
[ 2.367714] SPI driver ads7846 has no spi_device_id for ti,tsc2046
[ 2.373912] SPI driver ads7846 has no spi_device_id for ti,ads7843
[ 2.380188] SPI driver ads7846 has no spi_device_id for ti,ads7845
[ 2.386380] SPI driver ads7846 has no spi_device_id for ti,ads7873
[ 2.399700] rtc-pcf8523 0-0068: registered as rtc0
[ 2.406488] rtc-pcf8523 0-0068: hctosys: unable to read the hardware clock
[ 2.414663] snvs_rtc 20cc000.snvs:snvs-rtc-lp: registered as rtc1
[ 2.421071] i2c_dev: i2c /dev entries driver
[ 2.427714] pxp-v4l2 pxp_v4l2_out: initialized
[ 2.435616] Bluetooth: HCI UART driver ver 2.3
[ 2.440128] Bluetooth: HCI UART protocol H4 registered
[ 2.445275] Bluetooth: HCI UART protocol BCSP registered
[ 2.450650] Bluetooth: HCI UART protocol LL registered
[ 2.455818] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 2.462152] Bluetooth: HCI UART protocol Marvell registered
[ 2.467830] usbcore: registered new interface driver btusb
[ 2.474615] sdhci: Secure Digital Host Controller Interface driver
[ 2.480861] sdhci: Copyright(c) Pierre Ossman
[ 2.485226] sdhci-pltfm: SDHCI platform and OF driver helper
[ 2.500685] caam 2100000.crypto: Entropy delay = 12000
[ 2.507394] sdhci-esdhc-imx 219c000.mmc: Got CD GPIO
[ 2.546440] mmc2: SDHCI controller on 2198000.mmc [2198000.mmc] using ADMA
[ 2.553493] caam 2100000.crypto: Instantiated RNG4 SH0
[ 2.562312] mmc3: SDHCI controller on 219c000.mmc [219c000.mmc] using ADMA
[ 2.599089] caam 2100000.crypto: Instantiated RNG4 SH1
[ 2.604294] caam 2100000.crypto: device ID = 0x0a16010000000200 (Era 4)
[ 2.610978] caam 2100000.crypto: job rings = 2, qi = 0
[ 2.631280] caam algorithms registered in /proc/crypto
[ 2.638406] caam 2100000.crypto: rng crypto API alg registered prng-caam
[ 2.645251] caam 2100000.crypto: registering rng-caam
[ 2.652056] Device caam-keygen registered
[ 2.663672] caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state
[ 2.672680] usbcore: registered new interface driver usbhid
[ 2.678380] usbhid: USB HID core driver
[ 2.693577] wm8731 0-001a: Failed to issue reset: -6
[ 2.701227] fsl-ssi-dai 202c000.ssi: No cache defaults, reading back from HW
[ 2.711563] mmc2: new DDR MMC card at address 0001
[ 2.727138] mmcblk2: mmc2:0001 H8G4a2 7.28 GiB
[ 2.733841] mmcblk2: p1 p2
[ 2.744642] mmcblk2boot0: mmc2:0001 H8G4a2 8.00 MiB
[ 2.751228] mmcblk2boot1: mmc2:0001 H8G4a2 8.00 MiB
[ 2.767621] mmcblk2rpmb: mmc2:0001 H8G4a2 4.00 MiB, chardev (242:0)
[ 2.790691] random: crng init done
[ 2.904067] NET: Registered PF_LLC protocol family
[ 2.909553] NET: Registered PF_INET6 protocol family
[ 2.915834] Segment Routing with IPv6
[ 2.919647] In-situ OAM (IOAM) with IPv6
[ 2.923680] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 2.930275] NET: Registered PF_PACKET protocol family
[ 2.935442] can: controller area network core
[ 2.940055] NET: Registered PF_CAN protocol family
[ 2.944862] can: raw protocol
[ 2.947919] can: broadcast manager protocol
[ 2.952122] can: netlink gateway - max_hops=1
[ 2.956775] Bluetooth: RFCOMM TTY layer initialized
[ 2.961681] Bluetooth: RFCOMM socket layer initialized
[ 2.966969] Bluetooth: RFCOMM ver 1.11
[ 2.970743] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.976060] Bluetooth: BNEP filters: protocol multicast
[ 2.981392] Bluetooth: BNEP socket layer initialized
[ 2.986368] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.992329] Bluetooth: HIDP socket layer initialized
[ 2.997374] lib80211: common routines for IEEE802.11 drivers
[ 3.003086] Key type dns_resolver registered
[ 3.037116] Registering SWP/SWPB emulation handler
[ 3.042158] Loading compiled-in X.509 certificates
[ 3.070163] vddarm: supplied by SW1AB
[ 3.074526] vddsoc: supplied by SW1AB
[ 3.182138] sii902x bound to mxs-lcdif from 2220000.lcdif
[ 3.206075] Console: switching to colour frame buffer device 160x45
[ 3.331806] mxsfb 2220000.lcdif: initialized
[ 3.340029] imx_usb 2184000.usb: No over current polarity defined
[ 3.518815] imx_usb 2184200.usb: No over current polarity defined
[ 3.529042] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 3.533972] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1
[ 3.566473] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 3.572104] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.15
[ 3.580420] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 3.587668] usb usb1: Product: EHCI Host Controller
[ 3.592552] usb usb1: Manufacturer: Linux 5.15.32+geb06aa0de7de ehci_hcd
[ 3.599277] usb usb1: SerialNumber: ci_hdrc.1
[ 3.604262] hub 1-0:1.0: USB hub found
[ 3.608184] hub 1-0:1.0: 1 port detected
[ 3.627292] galcore: clk_get 2d core clock failed, disable 2d/vg!
[ 3.634306] Galcore version 6.4.3.p4.398061
[ 3.901547] [drm] Initialized vivante 1.0.0 20170808 for 1800000.gpu3d on minor 0
[ 3.912589] imx_thermal 20c8000.anatop:tempmon: Industrial CPU temperature grade - max:105C critical:100C passive:95C
[ 3.923457] Hot alarm is canceled. GPU3D clock will return to 64/64
[ 3.943113] clk: Not disabling unused clocks
[ 3.947537] ALSA device list:
[ 3.950517] No soundcards found.
[ 3.955248] Freeing unused kernel image (initmem) memory: 1024K
[ 3.961560] Run /linuxrc as init process
Found New UDC: ci_hdrc.0
ci_hdrc.0 0
ffs.utp0
[ 4.061237] file system registered
[ 4.092605] Mass Storage Function, version: 2009/09/11
[ 4.097996] LUN: removable file: (no medium)
run utp at /dev/usb-utp0/ep0
.
uuu fastboot client 1.0.0 [built [ 4.119109] read descriptors
Nov 7 2019 19:25:07]
Start init[ 4.126345] read strings
usb
.
write string
Start handle command
uuc /dev/utp
uuc 0.6 [built Nov 7 2019 19:25:07]
UTP: Waiting for /dev/utp to appear

 

However, when the kernel enters waiting mode, the uuu tool fails, as shown in
the log below:

uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-0-gaeb3490

Success 0 Failure 1


1:10 1/32 [Failure claim interface ] FBK: ucmd while [ ! -e /dev/mmcblk*boot0 ]; do sleep 1; echo "wait for /dev/mmcblk*boot* appear"; done;

 

After checking the output of dmesg on my host, I obtained the following:

[ +0.002880] hid-generic 0003:15A2:0071.0004: hiddev0,hidraw3: USB HID v1.10 Device [Freescale SemiConductor Inc SE Blank PELE] on usb-0000:00:14.0-10/input0
[Oct19 15:11] usb 1-10: USB disconnect, device number 5
[ +17.048879] usb 1-10: new full-speed USB device number 6 using xhci_hcd
[ +0.148392] usb 1-10: not running at top speed; connect to a high speed hub
[ +0.000391] usb 1-10: Duplicate descriptor for config 1 interface 0 altsetting 0, skipping
[ +0.000576] usb 1-10: New USB device found, idVendor=1fc9, idProduct=0152, bcdDevice= 2.21
[ +0.000013] usb 1-10: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000007] usb 1-10: Product: USB download gadget
[ +0.000004] usb 1-10: Manufacturer: FSL
[ +0.000004] usb 1-10: SerialNumber: bdf722c4bdf722c4
[Oct19 15:12] usb 1-10: USB disconnect, device number 6
[ +1.103440] usb 1-10: new full-speed USB device number 7 using xhci_hcd
[ +0.148671] usb 1-10: not running at top speed; connect to a high speed hub
[ +0.000738] usb 1-10: config 1 interface 0 altsetting 0 endpoint 0x81 has invalid wMaxPacketSize 0
[ +0.000012] usb 1-10: config 1 interface 0 altsetting 0 endpoint 0x1 has invalid wMaxPacketSize 0
[ +0.001254] usb 1-10: New USB device found, idVendor=066f, idProduct=9bff, bcdDevice= 5.15
[ +0.000013] usb 1-10: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000006] usb 1-10: Product: FSL i.MX Board
[ +0.000005] usb 1-10: SerialNumber: 0000000000000000
[ +0.000554] ================================================================================
[ +0.000009] UBSAN: shift-out-of-bounds in /build/linux-hwe-6.2-ZyAAgj/linux-hwe-6.2-6.2.0/include/linux/log2.h:67:13
[ +0.000009] shift exponent 4294967295 is too large for 64-bit type 'long unsigned int'
[ +0.000007] CPU: 6 PID: 11890 Comm: kworker/6:2 Tainted: P OE 6.2.0-34-generic #34~22.04.1-Ubuntu
[ +0.000009] Hardware name: Micro-Star International Co., Ltd. MS-7B98/Z390-A PRO (MS-7B98), BIOS 1.B0 08/10/2020
[ +0.000005] Workqueue: usb_hub_wq hub_event
[ +0.000012] Call Trace:
[ +0.000005] <TASK>
[ +0.000006] dump_stack_lvl+0x48/0x70
[ +0.000011] dump_stack+0x10/0x20
[ +0.000007] __ubsan_handle_shift_out_of_bounds+0x156/0x310
[ +0.000011] xhci_endpoint_init.cold+0x1e/0x34
[ +0.000015] xhci_add_endpoint.part.0+0x120/0x390
[ +0.000011] xhci_add_endpoint+0x41/0x80
[ +0.000009] usb_hcd_alloc_bandwidth+0x171/0x430
[ +0.000010] usb_set_configuration+0x10a/0xac0
[ +0.000007] ? kernfs_add_one+0xfc/0x140
[ +0.000009] ? kernfs_create_link+0x66/0xe0
[ +0.000010] usb_generic_driver_probe+0x6b/0xb0
[ +0.000011] usb_probe_device+0x38/0x130
[ +0.000008] really_probe+0x1ea/0x450
[ +0.000007] __driver_probe_device+0x8a/0x190
[ +0.000007] driver_probe_device+0x23/0xd0
[ +0.000006] __device_attach_driver+0xc5/0x160
[ +0.000006] ? __pfx___device_attach_driver+0x10/0x10
[ +0.000007] bus_for_each_drv+0x82/0xe0
[ +0.000009] __device_attach+0xc1/0x230
[ +0.000007] device_initial_probe+0x13/0x20
[ +0.000007] bus_probe_device+0x9b/0xb0
[ +0.000010] device_add+0x42a/0x700
[ +0.000008] usb_new_device+0x466/0x550
[ +0.000012] hub_port_connect+0x45b/0xbd0
[ +0.000008] hub_port_connect_change+0xa1/0x3c0
[ +0.000008] port_event+0x661/0x7f0
[ +0.000007] hub_event+0x157/0x450
[ +0.000006] ? __queue_delayed_work+0xcd/0xf0
[ +0.000010] process_one_work+0x21c/0x440
[ +0.000009] worker_thread+0x50/0x3f0
[ +0.000009] ? __pfx_worker_thread+0x10/0x10
[ +0.000007] kthread+0xeb/0x120
[ +0.000013] ? __pfx_kthread+0x10/0x10
[ +0.000010] ret_from_fork+0x29/0x50
[ +0.000011] </TASK>
[ +0.000003] ================================================================================
[ +0.002032] usb 1-10: can't set config #1, error -32

 

Flashing the same release with MfgTool on Windows works fine. Additionally,
flashing the same release on an older version of Ubuntu 18.04 on my coworker's
laptop also works fine. Does anyone have any idea what I'm doing wrong? Or is
there something wrong with my setup? I'm really confused here.

System info:

$ cat /etc/os-release
PRETTY_NAME="Ubuntu 22.04.3 LTS"
NAME="Ubuntu"
VERSION_ID="22.04"
VERSION="22.04.3 LTS (Jammy Jellyfish)"
VERSION_CODENAME=jammy
ID=ubuntu
ID_LIKE=debian
HOME_URL="https://www.ubuntu.com/"
SUPPORT_URL="https://help.ubuntu.com/"
BUG_REPORT_URL="https://bugs.launchpad.net/ubuntu/"
PRIVACY_POLICY_URL="https://www.ubuntu.com/legal/terms-and-policies/privacy-policy"
UBUNTU_CODENAME=jammy



Also, verbose output of uuu:

./uuu -v full_tar.uuu
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-0-gaeb3490

Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDPS: MX8ULP 0x1fc9 0x014a
SDPS: MX8ULP 0x1fc9 0x014b
SDPS: MX93 0x1fc9 0x014e
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPV: SPL1 0x1fc9 0x0151 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FBK: 0x1fc9 0x0153
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
FB: 0x1fc9 0x0152
FB: 0x0483 0x0afb
Wait for Known USB Device Appear...
New USB Device Attached at 1:10
1:10>Start Cmd:SDP: boot -f firmware/u-boot.imx
100%1:10>Okay (1.133s)
New USB Device Attached at 1:10
1:10>Start Cmd:FB: ucmd setenv fastboot_dev mmc
1:10>Okay (0.001s)
1:10>Start Cmd:FB: ucmd setenv mmcdev ${emmc_dev}
1:10>Okay (0s)
1:10>Start Cmd:FB: ucmd mmc dev ${emmc_dev}
1:10>Okay (0.031s)
1:10>Start Cmd:FB: ucmd setenv fastboot_buffer ${loadaddr}
1:10>Okay (0.001s)
1:10>Start Cmd:FB: download -f firmware/zImage
1:10>Okay (8.161s)
1:10>Start Cmd:FB: ucmd setenv fastboot_buffer ${fdt_addr}
1:10>Okay (0s)
1:10>Start Cmd:FB: download -f firmware/kit_v2.dtb
1:10>Okay (0.05s)
1:10>Start Cmd:FB: ucmd setenv fastboot_buffer ${initrd_addr}
1:10>Okay (0.001s)
1:10>Start Cmd:FB: download -f firmware/fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot
1:10>Okay (11.02s)
1:10>Start Cmd:FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}
1:10>Okay (0s)
New USB Device Attached at 1:10
1:10>Start Cmd:FBK: ucmd while [ ! -e /dev/mmcblk*boot0 ]; do sleep 1; echo "wait for /dev/mmcblk*boot* appear"; done;
1:10>Fail Failure claim interface(0s)

 

0 项奖励
回复
1 解答
934 次查看
andriibr
Contributor II

The issue ended up being related to the kernel image inside the initramfs used during flashing, not to the uuu tool itself. I tried kernels from different releases and managed to flash the board with an older one.

The uuu_imx6sx_com_4.14.78 release worked.

在原帖中查看解决方案

3 回复数
935 次查看
andriibr
Contributor II

The issue ended up being related to the kernel image inside the initramfs used during flashing, not to the uuu tool itself. I tried kernels from different releases and managed to flash the board with an older one.

The uuu_imx6sx_com_4.14.78 release worked.

1,237 次查看
Alejandro_Salas
NXP TechSupport
NXP TechSupport

Hello @andriibr !

 

I was checking the documentation and zip file where is contained the BSP for the i.MX6SX from Embedded Artist and I could see the UUU script is validated with tool version 1.4.243:

Alejandro_Salas_0-1697729003826.png

Also, I could see you are using a newer version (1.5.125).

 

Could you please try to run the below command with UUU 1.4.243 version?

$ sudo ./uuu full_tar.uuu

 

Please try it and let me know how it was.

 

Best regards!

0 项奖励
回复
1,220 次查看
andriibr
Contributor II

Thanks for the quick reply @Alejandro_Salas

I just tried the 1.4.243, but results are still the same

$ ./uuu full_tar.uuu
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.243-0-ged48c51

Success 0 Failure 1


1:10 1/32 [Failure claim interface ] FBK: ucmd while [ ! -e /dev/mmcblk*boot0 ]; do sleep 1; echo "wait for /dev/mmcblk*boo


The kernel panic I attached earlier, also occurred on my host again.

[ +0.003931] hid-generic 0003:15A2:0071.0004: hiddev0,hidraw3: USB HID v1.10 Device [Freescale SemiConductor Inc SE Blank PELE] on usb-0000:00:14.0-10/input0
[ +1.435968] usb 1-10: USB disconnect, device number 5
[ +15.245998] usb 1-10: new full-speed USB device number 6 using xhci_hcd
[ +0.148297] usb 1-10: not running at top speed; connect to a high speed hub
[ +0.000363] usb 1-10: Duplicate descriptor for config 1 interface 0 altsetting 0, skipping
[ +0.000486] usb 1-10: New USB device found, idVendor=1fc9, idProduct=0152, bcdDevice= 2.21
[ +0.000008] usb 1-10: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000003] usb 1-10: Product: USB download gadget
[ +0.000003] usb 1-10: Manufacturer: FSL
[ +0.000002] usb 1-10: SerialNumber: bdf722c4bdf722c4
[ +23.833569] usb 1-10: USB disconnect, device number 6
[ +1.080403] usb 1-10: new full-speed USB device number 7 using xhci_hcd
[ +0.148603] usb 1-10: not running at top speed; connect to a high speed hub
[ +0.000729] usb 1-10: config 1 interface 0 altsetting 0 endpoint 0x81 has invalid wMaxPacketSize 0
[ +0.000013] usb 1-10: config 1 interface 0 altsetting 0 endpoint 0x1 has invalid wMaxPacketSize 0
[ +0.001247] usb 1-10: New USB device found, idVendor=066f, idProduct=9bff, bcdDevice= 5.15
[ +0.000013] usb 1-10: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000006] usb 1-10: Product: FSL i.MX Board
[ +0.000005] usb 1-10: SerialNumber: 0000000000000000
[ +0.000490] ================================================================================
[ +0.000010] UBSAN: shift-out-of-bounds in /build/linux-hwe-6.2-ZyAAgj/linux-hwe-6.2-6.2.0/include/linux/log2.h:67:13
[ +0.000009] shift exponent 4294967295 is too large for 64-bit type 'long unsigned int'
[ +0.000007] CPU: 4 PID: 48771 Comm: kworker/4:2 Tainted: P OE 6.2.0-34-generic #34~22.04.1-Ubuntu
[ +0.000009] Hardware name: Micro-Star International Co., Ltd. MS-7B98/Z390-A PRO (MS-7B98), BIOS 1.B0 08/10/2020
[ +0.000004] Workqueue: usb_hub_wq hub_event
[ +0.000013] Call Trace:
[ +0.000005] <TASK>
[ +0.000005] dump_stack_lvl+0x48/0x70
[ +0.000012] dump_stack+0x10/0x20
[ +0.000006] __ubsan_handle_shift_out_of_bounds+0x156/0x310
[ +0.000014] xhci_endpoint_init.cold+0x1e/0x34
[ +0.000012] xhci_add_endpoint.part.0+0x120/0x390
[ +0.000014] xhci_add_endpoint+0x41/0x80
[ +0.000009] usb_hcd_alloc_bandwidth+0x171/0x430
[ +0.000009] usb_set_configuration+0x10a/0xac0
[ +0.000007] ? kernfs_add_one+0xfc/0x140
[ +0.000009] ? kernfs_create_link+0x66/0xe0
[ +0.000010] usb_generic_driver_probe+0x6b/0xb0
[ +0.000011] usb_probe_device+0x38/0x130
[ +0.000007] really_probe+0x1ea/0x450
[ +0.000008] __driver_probe_device+0x8a/0x190
[ +0.000006] driver_probe_device+0x23/0xd0
[ +0.000006] __device_attach_driver+0xc5/0x160
[ +0.000007] ? __pfx___device_attach_driver+0x10/0x10
[ +0.000006] bus_for_each_drv+0x82/0xe0
[ +0.000010] __device_attach+0xc1/0x230
[ +0.000007] device_initial_probe+0x13/0x20
[ +0.000006] bus_probe_device+0x9b/0xb0
[ +0.000010] device_add+0x42a/0x700
[ +0.000009] usb_new_device+0x466/0x550
[ +0.000011] hub_port_connect+0x45b/0xbd0
[ +0.000008] hub_port_connect_change+0xa1/0x3c0
[ +0.000008] port_event+0x661/0x7f0
[ +0.000008] hub_event+0x157/0x450
[ +0.000006] ? psi_avgs_work+0x61/0xd0
[ +0.000013] process_one_work+0x21c/0x440
[ +0.000014] worker_thread+0x50/0x3f0
[ +0.000008] ? __pfx_worker_thread+0x10/0x10
[ +0.000008] kthread+0xeb/0x120
[ +0.000010] ? __pfx_kthread+0x10/0x10
[ +0.000010] ret_from_fork+0x29/0x50
[ +0.000011] </TASK>
[ +0.000002] ================================================================================
[ +0.002068] usb 1-10: can't set config #1, error -32
[ +12.396430] audit: type=1400 audit(1697788916.352:133): apparmor="DENIED" operation="open" class="file" profile="snap.firefox.firefox" name="/etc/fstab" pid=3178 comm="firefox" requested_mask="r" denied_mask="r" fsuid=1000 ouid=0


[ +0.003931] hid-generic 0003:15A2:0071.0004: hiddev0,hidraw3: USB HID v1.10 Device [Freescale SemiConductor Inc SE Blank PELE] on usb-0000:00:14.0-10/input0
[ +1.435968] usb 1-10: USB disconnect, device number 5
[ +15.245998] usb 1-10: new full-speed USB device number 6 using xhci_hcd
[ +0.148297] usb 1-10: not running at top speed; connect to a high speed hub
[ +0.000363] usb 1-10: Duplicate descriptor for config 1 interface 0 altsetting 0, skipping
[ +0.000486] usb 1-10: New USB device found, idVendor=1fc9, idProduct=0152, bcdDevice= 2.21
[ +0.000008] usb 1-10: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000003] usb 1-10: Product: USB download gadget
[ +0.000003] usb 1-10: Manufacturer: FSL
[ +0.000002] usb 1-10: SerialNumber: bdf722c4bdf722c4
[ +23.833569] usb 1-10: USB disconnect, device number 6
[ +1.080403] usb 1-10: new full-speed USB device number 7 using xhci_hcd
[ +0.148603] usb 1-10: not running at top speed; connect to a high speed hub
[ +0.000729] usb 1-10: config 1 interface 0 altsetting 0 endpoint 0x81 has invalid wMaxPacketSize 0
[ +0.000013] usb 1-10: config 1 interface 0 altsetting 0 endpoint 0x1 has invalid wMaxPacketSize 0
[ +0.001247] usb 1-10: New USB device found, idVendor=066f, idProduct=9bff, bcdDevice= 5.15
[ +0.000013] usb 1-10: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000006] usb 1-10: Product: FSL i.MX Board
[ +0.000005] usb 1-10: SerialNumber: 0000000000000000
[ +0.000490] ================================================================================
[ +0.000010] UBSAN: shift-out-of-bounds in /build/linux-hwe-6.2-ZyAAgj/linux-hwe-6.2-6.2.0/include/linux/log2.h:67:13
[ +0.000009] shift exponent 4294967295 is too large for 64-bit type 'long unsigned int'
[ +0.000007] CPU: 4 PID: 48771 Comm: kworker/4:2 Tainted: P OE 6.2.0-34-generic #34~22.04.1-Ubuntu
[ +0.000009] Hardware name: Micro-Star International Co., Ltd. MS-7B98/Z390-A PRO (MS-7B98), BIOS 1.B0 08/10/2020
[ +0.000004] Workqueue: usb_hub_wq hub_event
[ +0.000013] Call Trace:
[ +0.000005] <TASK>
[ +0.000005] dump_stack_lvl+0x48/0x70
[ +0.000012] dump_stack+0x10/0x20
[ +0.000006] __ubsan_handle_shift_out_of_bounds+0x156/0x310
[ +0.000014] xhci_endpoint_init.cold+0x1e/0x34
[ +0.000012] xhci_add_endpoint.part.0+0x120/0x390
[ +0.000014] xhci_add_endpoint+0x41/0x80
[ +0.000009] usb_hcd_alloc_bandwidth+0x171/0x430
[ +0.000009] usb_set_configuration+0x10a/0xac0
[ +0.000007] ? kernfs_add_one+0xfc/0x140
[ +0.000009] ? kernfs_create_link+0x66/0xe0
[ +0.000010] usb_generic_driver_probe+0x6b/0xb0
[ +0.000011] usb_probe_device+0x38/0x130
[ +0.000007] really_probe+0x1ea/0x450
[ +0.000008] __driver_probe_device+0x8a/0x190
[ +0.000006] driver_probe_device+0x23/0xd0
[ +0.000006] __device_attach_driver+0xc5/0x160
[ +0.000007] ? __pfx___device_attach_driver+0x10/0x10
[ +0.000006] bus_for_each_drv+0x82/0xe0
[ +0.000010] __device_attach+0xc1/0x230
[ +0.000007] device_initial_probe+0x13/0x20
[ +0.000006] bus_probe_device+0x9b/0xb0
[ +0.000010] device_add+0x42a/0x700
[ +0.000009] usb_new_device+0x466/0x550
[ +0.000011] hub_port_connect+0x45b/0xbd0
[ +0.000008] hub_port_connect_change+0xa1/0x3c0
[ +0.000008] port_event+0x661/0x7f0
[ +0.000008] hub_event+0x157/0x450
[ +0.000006] ? psi_avgs_work+0x61/0xd0
[ +0.000013] process_one_work+0x21c/0x440
[ +0.000014] worker_thread+0x50/0x3f0
[ +0.000008] ? __pfx_worker_thread+0x10/0x10
[ +0.000008] kthread+0xeb/0x120
[ +0.000010] ? __pfx_kthread+0x10/0x10
[ +0.000010] ret_from_fork+0x29/0x50
[ +0.000011] </TASK>
[ +0.000002] ================================================================================
[ +0.002068] usb 1-10: can't set config #1, error -32
[ +12.396430] audit: type=1400 audit(1697788916.352:133): apparmor="DENIED" operation="open" class="file" profile="snap.firefox.firefox" name="/etc/fstab" pid=3178 comm="firefox" requested_mask="r" denied_mask="r" fsuid=1000 ouid=0
0 项奖励
回复