Cannot find vold.fstab

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Cannot find vold.fstab

5,053 Views
jonathansmyth
Contributor III

Hi Guys,

Im looking for the vold.fstab to make modifactions to so i can flash android JB4.3 to a custom board it runs imx6dl

i have added my custom board everything compiles...but when igo to look for the file which should be in device / fsl / sabreauto_6q its not there...

-dev_mount EXTSD / mnt / EXTSD car /devices/platform/sdhci-esdhc-imx.0/mmc_host/mmc1/

+ Dev_mount EXTSD / mnt / EXTSD car /devices/platform/sdhci-esdhc-imx.2/mmc_host/mmc0/


i need to make these changes for my custom board ^^


and these in imx6/etc/init.rc


+ # Hold WAKE_LOCK as the android system will not suspend (suspend is not here Desired)

+ Write / sys / power / WAKE_LOCK temporary


however my predesscor wasnt very clear in his documentation...any help would be greatly appreciated!!



Thanks Jonny

Labels (3)
0 Kudos
Reply
0 Replies