Hi Qiang,
Are you using the BSP provided by freescale? In the i.MX_6_SABRE-SD_Linux_User's_Guide.pdf document, you can see details on 6.2 Download Images by U-Boot. Take the BSP L3.10.17_1.0.0 as an example, you can refer to the attachment file.
Hope this can help you. Any questions you can contact me easily.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Qiang Wang,
What platform and which version of BSP are you using?
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
yocto imx6qsabresd uboot(2014.02)
Hi Qiang,
Are you using the BSP provided by freescale? In the i.MX_6_SABRE-SD_Linux_User's_Guide.pdf document, you can see details on 6.2 Download Images by U-Boot. Take the BSP L3.10.17_1.0.0 as an example, you can refer to the attachment file.
Hope this can help you. Any questions you can contact me easily.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Dan:
我的问题是:
假如EMMC没有分区,我想在UBOOT中给EMMC分2个分区
6.2讲的是EMMC启动以及在内核中分区
Hi Qiang,
Have you solved your questions, if yes please help click the Correct Answer button, thank you.
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Dear Dan:
谢谢你的及时回复,看来只能自己移植命令进去了!!!
Hi Qiang,
不客气的:smileyhappy:,欢迎有问题继续在本论坛中创建提问哈~~
Have a nice day
Best Regards
Dan
Hi Qiang,
是要在内核启动以后,分区的命令才可以使用,我刚跟别的同事确认了一下,在u-boot中对EMMC分区的话是不可以的,没有命令可以使用。不过这是针对2012以及以前的版本,新版本2014版本的u-boot我们这边不是很清楚。
这里还是建议你使用NFS启动,或者是我上述给你的方法,对EMMC分区。希望对你有帮助。
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------