Cannot Find the "i.MX Linux User's Guide"

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot Find the "i.MX Linux User's Guide"

5,427 次查看
cbrust
Contributor III

The "i.MX Linux User's Guide" is referenced in several documents including the "Freescale Yocto Project User's Guide".  However, I am unable to locate this document anywhere.  Can someone direct me to the document? 

Here's the reference pulled from the Freescale Yocto Project User's Guide.

Appendix B References

For details on boot switches, see Section "How to Boot the i.MX Boards" in the

i.MX Linux User's Guide

For how to download images using U-boot, see Section "Downloading Images Using U-Boot" in the

i.MX Linux User's Guide

For how to set up an SD/MMC card, see Section "Preparing an SD/MMC Card to Boot" in the

i.MX Linux User's Guide

标签 (3)
0 项奖励
回复
1 回复

1,322 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Brust

Linux User Guide is included in Doc Bundle for each BSP (also please find it attached)

Board Support Packages (27)

L3.14.28_1.0.0_iMX6QDLS_BUNDLE (REV L3.14.28_1.0.0)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREBRD&fpsp=1&tab=Design_Tool...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------