I want to use iMx6Solo. I have gone through i.MX 6Solo/6DualLite Applications Processor Reference Manual, Rev. 5, 05/2020 Page 209. Document is saying Feature that : Nand-Flash (MLC up to 40-bit ECC) and NOR Flash memory interface via GPMI Nand-Flash controller.
But After going through GPMI chapter in detail I didn't found NOR Flash.
So my question is "Can we use 64MB NOR Flash with iMX6solo GPMI interface?"
If we want to use SPI NOR Flash as Boot Flash then what will be max size SPI NOR Flash in iMx6Solo?