Can the iMX8M support the CS42888 in linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can the iMX8M support the CS42888 in linux

Jump to solution
909 Views
nathani
Contributor II

Can the iMX8M support the CS42888 audio codec in yocto linux, or is support only for SOCs with ESAI support at the moment?

https://github.com/Freescale/linux-fslc/blob/4.14-2.0.x-imx/Documentation/devicetree/bindings/sound/...

The device tree file says to specify "The phandle of the i.MX SSI controller", but the variable is "esai-controller"...

The iMX8M-Mini has "one SAI with 4 TX and 4 RX lanes" that seems a good fit, can you just pull down the 2 unused pins? 

Thanks,

Nathan

1 Solution
794 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

you are right currently it is supported only for SOCs with ESAI, no support for i.MX8M.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
795 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nathan

you are right currently it is supported only for SOCs with ESAI, no support for i.MX8M.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------