Can the i.MX6Solo drive 2 x 1080P30 displays via LVDS?
Hi James
not, as perfomance described in sect.40.4.1 Input Parallel Display Ports
i.MX6SDL Reference Manual (rev.2 5/2015):
for dual input data interface case :
Up to 85 MHz per interface. (WXGA 1366x768 @
60 frames per second, 35% blanking)
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Thanks for the response.
However, for external displays, wouldn’t this be an Output LVDS Port?
James
Hi
"dual input data interface" means that
it will be outputed on two separate LVDS Ports.
Best regards
igor