when did the "i.mx6-scm" single chip module industrial temperature level product release?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

when did the "i.mx6-scm" single chip module industrial temperature level product release?

844件の閲覧回数
wyb3360132
Contributor I

When did the "i.mx6-scm" single chip module industrial temperature level product release?

I find the  industrial grade product order number at arrow site  was " MSCMMX6DZCK08AB1G0A"

flow the naming rule in the other imx6 chip, MSCMMX6DZ"C" the C character mean this chip was industrial grade, am i right?

But i can't make sure this order number was right, because nxp site did not have the industrial datasheet about this chip.

someone help me.

0 件の賞賛
返信
1 返信

732件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi wang

SCM-i.MX 6Dual and SCM-i.MX 6 Quad industrial devices are sampling.

Production in 4Q 2016. Arrow naming rules are different.

For nxp please refer to

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQIEC.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信