Trying to Build Android KK 4.4.3_2 for iMX6 SabreSD board.
Using Ubuntu 14.04 LTS as host environment.
I have been able to successfully build and run Android KK for Sabre lite board using instructions from http://boundarydevices.com/android-kitkat-second-release-mx6-boards/. This would seems to say that my host machine is setup correctly for building Android.
I want build a Android install for the IMX6 using FreeScales build instructions. I am following the Freescale Android User's Guide (Rev KK4.4.3_2.0.0-ga, 2/2015 found here
i.MX 6 Series Software and Development Tool R|Freescale and
IMX6_KK443_200_ANDROID_SOURCE_BSP
Steps I completed from Section 3)
$ cd ~
$ mkdir myandroid
$ mkdir bin
$ cd myandroid
$ curl http://commondatastorage.googleapis.com/git-repo-downloads/repo > ~/bin/repo
$ chmod a+x ~/bin/repo
$ ~/bin/repo init -u https://android.googlesource.com/platform/manifest -b android-4.4.3_r1
$ ~/bin/repo sync # this command loads most needed repos. Therefore, it can take several
hours to load.
Get KK4.4.3_2.0.0-ga kernel source code from Freescale open source git:
$ cd myandroid
$ git clone git://git.freescale.com/imx/linux-2.6-imx.git kernel_imx # the kernel repo is
heavy. Therefore, this process can take a while.
$ cd kernel_imx
$ git checkout kk4.4.3_2.0.0-ga
$ cd myandroid/bootable
$ cd bootloader
$ git clone git://git.freescale.com/imx/uboot-imx.git uboot-imx
$ cd uboot-imx
$ git checkout kk4.4.3_2.0.0-ga
$ cd ~/myandroid
$ source /opt/android_KK4.4.3_2.0.0-ga_core_source/code/KK4.4.3_2.0.0-ga/and_patch.sh
$ c_patch /opt/android_KK4.4.3_2.0.0-ga_core_source/code/KK4.4.3_2.0.0-ga
imx_KK4.4.3_2.0.0-ga
3. If everything is OK, "c_patch" will generate the following output to indicate the successful patch:
**************************************************************
Success: Now you can build the Android code for FSL i.MX platform
**************************************************************
I get the correct output.. All looks Good...
$ cd ~/myandroid
$ source build/envsetup.sh
$ lunch sabresd_6dq-user
The Last Command FAILS!..
After investigation it does NOT look like the PATCH completed..
For example
myandriod/devices/fsl is not populated
user@ubuntu:/opt/Android/myandroid/device/fsl$ ls -la
total 12
drwxrwxr-x 3 user user 4096 Mar 25 15:02 .
drwxrwxr-x 11 user user 4096 Mar 25 15:02 ..
-rw-rw-r-- 1 user user 0 Mar 25 15:02 .dummy
drwxrwxr-x 8 user user 4096 Mar 25 15:02 .git
In myandroid/kernel_imx/arch/arm/
I would expect a mx6 subdirectory.. This is missing.
I have done the complete process 2 times..
What Am I missing?
Thanks
I have downloaded android_jb4.3_1.1.0-ga_source and unzipped into /opt folder. But I am getting Base commit version errors. Could you suggest me the correct imx patch for Android 4.3_r2.1 version.
Hi Bill,
I have followed the same process as you mentioned in the same post. After I downloaded the android source code repo from the below mentioned website: http://commondatastorage.googleapis.com/git-repo-downloads/repo
I don't have opt folder in myandroid folder. Could you help me with this ?
Sergio:
Thanks for the answer.. I believe I tried that.
To answer my own thread.. I got it to work by going back 12.04 LTS.. (and a lot of setup and apt-get).. As many many others threads have talked about it ussually relates to Java version.
I got Linux Android to work and run on Sabre SD.
After a week, Still no assistance from Freescale.. :smileyconfused:
However, I have an update.
I built a new Unbuntu VM machine based on 12.04 LTS 64bit.. Running the c_patch command seems to have worked. It appears that the SED/AWK commands in the scripts fail in 14.04 LTS . In 12.04 LTS version c_patch displays line after line of comments about "Newline" terminations..
New VM machine (12.04) didnt have java JDK working correctly, even though I followed the prereq as described in the FreeScale Android Guide & https://community.freescale.com/docs/DOC-98441
This is what worked for me (found in comments)
The "deb http://archive.canonical.com/ lucid partner" source doesn't work. Try:
$ sudo add-apt-repository "deb http://ppa.launchpad.net/ferramroberto/java/ubuntu natty main"
$ sudo apt-get update
$ sudo apt-get install sun-java6-jdk
Would be nice to understand:
- Why C_PATCH works for 12.04 but not 14.04
- Fix the Final banner that says it completed correctly when it clearly didn't
$"make" is currently blowing up pretty quick along the way but I believe that is because I don't have all the needed tools installed yet.. wish me luck
Hello Bill,
There is a document that explains step by step how to build android using ubuntu 14.04 as a host.
[GUIDE] Setup Android Development Environment on Ubuntu 14.04 Trusty Tahr
Please take a look at it, you can guide by it.