HI,
Can imx6solo support ISL79985 ‘s 4 camera in?
We use intersil's isl79985-mipi to camputre 4 D1 camera video to imx6solo's 2 mipi lane,can imx6solo support?
I know IMX6Q support ISL79985 by its 4 lane,but IMX6SOLO only has 2lane and 2 virtual channel.
can imx6solo support isl79986-bt656 interface?where is the driver?
thanks.
ISL79985 datasheet is following:
ISL79985 | Video Decoders | Intersil
Hi
attached sensor has 2 lanes which should be fine for i.MX6S.
4 cameras can be processed as in below
since i.MX6S has only two CSI (one IPU), this could not be fully implemented. Seems it could
be processed in generic format, with further processing in software. I am not aware of efforts
for developing driver for this sensor.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
HI,
thanks a lot.
Do you mean imx6s can not support isl79985?
If isl79985 can mix 4camera video to one virtual channel,do imx6s can support it?
> If isl79985 can mix 4camera video to one virtual channel,do imx6s can support it?
yes