Hi everyone.
I want to install Atheros mini-PCIe wifi card on i.MX6dl sabresd board.
But i can not solve wifi error.
I was set configure below...
1. menuconfig set.
check [*]
Bus support -> PCI support,
Message Signaled Interrupts(MSi...MSI-x)
PCI Express port BUS support
PCI host controller drivers -> Freescale i.MX6 PCIe controller .
Device Driver -> Network device support --> Wireless LAN ->
Atheros Wireless Cards -> Atheros 802.11ac wireless cards support -> Atheros ath10k PCI support ..done.
2. package set
$build/conf/local.conf
Add text for wifi install like below...
IMAGE_INSTALL_append += " iw wpa-supplicant net-tools ethtool pciutils \
modutils-initscripts i2c-tools wireless-tools kernel-modules"
3. Compile and mount to target board(i.mx6dl sabresd)
4. copy firmware
cp firmware-2.bin_10.1.467.2-1 /lib/firmware/ath10k/QCA988X/hw2.0/firmware-2.bin
and reboot.
But can not work wifi card.
attached file is boot log for sabresd board.
Can i have solution?
Original Attachment has been moved to: boot_ath10k_wificard_error.log.zip
Hi Hanseung
from log "ath10k: could not probe fw"
this may be incompatibility firmware with this modem
model/linux versions, so one can try to ask updated
firmware from atheros support.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------