Can i.MX6ULL support NAND and SRAM?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i.MX6ULL support NAND and SRAM?

ソリューションへジャンプ
1,014件の閲覧回数
w2vy
Contributor V

We are looking at the i.MX6ULL and want to boot from NAND Flash and use it for file storage but we also need to use EIM to access SRAM.

We will not be using Linux

Using the PIn Mux tool if we enable the NAND interface a number of address lines of EIM are not available.

Still available are:

eim_ad0-ad7

eim_addr18-24

eim_cs0,2,3

eim_data0-15

eim_lba

eim_oe

eim_rw

This seems to all but cripple using the EIM for anything other than very small I/O areas.

I hope I am missing something

Tom

タグ(3)
0 件の賞賛
返信
1 解決策
795件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tom

you are right, as there are no much alternate pin mux options

for both interfaces, as described in sect.4.1.1 Muxing Options,

Table 8-9. EIM IOMUX pin configuration i.MX6UL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

If both interfaces are not used simultaneously one can consider to reconfigure

muxing in application, probably adding some isolation circuit, example of such

circuit can be found in p.13 spf-27452 i.MX6SL EVK schematic:

Schematics (2)
Design files, including hardware schematics, Gerbers, and OrCAD files. (REV 1)
i.MX 6SoloLite Evaluation Kit|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
796件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tom

you are right, as there are no much alternate pin mux options

for both interfaces, as described in sect.4.1.1 Muxing Options,

Table 8-9. EIM IOMUX pin configuration i.MX6UL Reference Manual

http://www.nxp.com/docs/en/reference-manual/IMX6ULLRM.pdf 

If both interfaces are not used simultaneously one can consider to reconfigure

muxing in application, probably adding some isolation circuit, example of such

circuit can be found in p.13 spf-27452 i.MX6SL EVK schematic:

Schematics (2)
Design files, including hardware schematics, Gerbers, and OrCAD files. (REV 1)
i.MX 6SoloLite Evaluation Kit|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------