We have a MX8QM board (with Yocto BSP 4.19.35) with two LVDS outputs( LVDS-1 and LVDS-2),
both with the same resolution 800x480@30fps.
And the application needs to output duplicate content on these two different LVDS displays.
On MX6Q, output LVDS ports can be used as:
"Two identical outputs: single input sent to both output channels".
This is exactly what we need.
Can MX8QM LVDS output ports support the same mode ?
If not, how can I get two different LVDS displays to output the same content on MX8QM SoC?
Regards,
Robbie