Can MX8QM support duplicate outputs on two LVDS displays?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can MX8QM support duplicate outputs on two LVDS displays?

671件の閲覧回数
RobbieJiang
Contributor IV


We have a MX8QM board (with Yocto BSP 4.19.35) with two LVDS outputs( LVDS-1 and LVDS-2),
both with the same resolution 800x480@30fps.

And the application needs to output duplicate content on these two different LVDS displays.

On MX6Q, output LVDS ports can be used as:
"Two identical outputs: single input sent to both output channels".
This is exactly what we need.

Can MX8QM LVDS output ports support the same mode ?

If not, how can I get two different LVDS displays to output the same content on MX8QM SoC?

 

Regards,

Robbie

0 件の賞賛
2 返答(返信)

661件の閲覧回数
RobbieJiang
Contributor IV
0 件の賞賛

653件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

yes you can refer to this

0 件の賞賛