Hi Friends,
According to part "Table 66. Camera Input Signal Cross Reference, Format, and Bits Per Cycle" in IMX6DQPAEC.pdf
BT.656 data should be feed in IPUx_CSIx_DATA[19:12].
But in my application, i need at least one BT.656 port input, one BT.1120 port input and at least 3 UARTS. most of UARTS share pins on IPUx_CSIx_DATA[19:12]. So i want to use IPUx_CSIx_DATA[9:2] to capture BT.656. Does it make sense by changing software?
Thanks
James He
已解决! 转到解答。
No, this is not possible. The camera should always be connected to the upper lines of the parallel CSI bus.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
No, this is not possible. The camera should always be connected to the upper lines of the parallel CSI bus.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------