Can I build a my custom libEGL library?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I build a my custom libEGL library?

622 Views
hyunwoolee
Contributor II

Hello.

I work with i.MX6Q Auto with Linux BSP (L3.0.35_4.0.0_130424_source).

I have to modify fbCreateFunction in libEGL-fb.so but I can't find the build package.

In result of tracing of that, there was http://bitshrine.org/gpp/gpu-viv-src-12.09.01.tar.gz

but the link is not alive now.

I want to add some codes at the start of fbCreateWindow function, not vivante driver.

Is that freescale's property or should be opened to all as opensource result?

Please help me.

Thanks

0 Kudos
1 Reply

426 Views
igorpadykov
NXP Employee
NXP Employee

Hi, Hyunwoo

Vivante GPU sources are closed for customers (under NDA), please

enter ticket to Freescale support for obtaining more details how one can get it.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos