Can I build a my custom libEGL library?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can I build a my custom libEGL library?

1,172件の閲覧回数
hyunwoolee
Contributor II

Hello.

I work with i.MX6Q Auto with Linux BSP (L3.0.35_4.0.0_130424_source).

I have to modify fbCreateFunction in libEGL-fb.so but I can't find the build package.

In result of tracing of that, there was http://bitshrine.org/gpp/gpu-viv-src-12.09.01.tar.gz

but the link is not alive now.

I want to add some codes at the start of fbCreateWindow function, not vivante driver.

Is that freescale's property or should be opened to all as opensource result?

Please help me.

Thanks

0 件の賞賛
返信
1 返信

976件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi, Hyunwoo

Vivante GPU sources are closed for customers (under NDA), please

enter ticket to Freescale support for obtaining more details how one can get it.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信