Can Freescale publish its deb packages' build procedure in its BSP and its Ubuntu release?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can Freescale publish its deb packages' build procedure in its BSP and its Ubuntu release?

824 次查看
YuLin
Contributor I

Can Freescale publish its deb packages' build procedure in its BSP and its Ubuntu release 10.04?

 

On i.mx51, and i.mx53.

Packages, gstreamer and others~~~.

 

It is very useful to compile those packages on other Ubuntu release 11.05 or 11.06 from community linaro.

 

Two reference I found. But I failed to do gstreamer install on linaro 11.06 ubuntu desktop.

http://boundarydevices.com/blogs/building-gstreamer-plugins-under-ubuntu

http://boundarydevices.com/blogs/freescale-gstreamer-plugins

 

Compile succeed. Install seems ok. Finally gplay and totem both failed. :(

标记 (1)
0 项奖励
回复
1 回复

710 次查看
JiJianFeng
Contributor I

  There are one section 1.2 Installing/Building the Plugins on Ubuntu in Linux_Multimedia_Framework_User_Guide.pdf, which described how to build the gstreamer plugins on Ubuntu Lucid rootfs but it is only for native build and only for multimedia level. The BSP level packages are generated from rpm package.

  The gstreamer related debian packages for Linaro 11.05 are located in one private PPA. I am not sure how to distribute it, I will check it.  Anyway all the gstreamer related packages should can be build in linaro rootfs, but for better performance, one patch for gstreamer base package should be applied ( because of different gstreamer core version).

0 项奖励
回复